calculate time interval (stm32f405 rgt6)
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-09-29 10:39 PM
My work on stm32f405 just started last month. It means I don't know very much about it, and I have been working on other C/C++ applications development.
The stm32 MCU board I have is given in snapshots.
I have been working on time interval's computation for almost one week but no good idea to get it.
I tried using SysTick->VAL and RTC but doesn't work, for I was told that there is no RTC on the board and SysTick needs to reload which had been initialized at the very beginning of the system for some delays(). In this case, there is no simple way for me to do this. Someone has told me to use TIM but 4 TIM (2 to 5) were used for encoders, and I'am worrying about doing configurations for hardware because of wick knowledge in hardware. So, anyone help?
SysTick's init is done after system startup
void delay_init(168)
{
#if SYSTEM_SUPPORT_OS .
u32 reload;
#endif
SysTick_CLKSourceConfig(SysTick_CLKSource_HCLK_Div8);
fac_us=SYSCLK/8;
#if SYSTEM_SUPPORT_OS
reload=SYSCLK/8;
reload*=1000000/delay_ostickspersec;
fac_ms=1000/delay_ostickspersec;
SysTick->CTRL|=SysTick_CTRL_TICKINT_Msk;
SysTick->LOAD=reload;
SysTick->CTRL|=SysTick_CTRL_ENABLE_Msk;
#else
fac_ms=(u16)fac_us*1000;
#endif
}
- Labels:
-
STM32F4 Series