2013-10-09 1:43 AM
Hi.
I am designing a test board using STM32F0 series MCU.On the datasheet, it states I have to attach 3 bypass capacitors(2 x 0.1uF, 1 x 4.7 uF) per each VDD. Is it absolutely necessary?, What is the point of using two identical capacitor, when I can use a single capacitor with about 0.2uF value? so that I only have to use 2 capacitors per each VDD pin saving me the board real-estate?Anyone have ideas??Thank you.2013-10-09 1:53 AM
Hello188
You've just misread it. It's one 0.1uF per Vdd pin (local de-coupling) and a single 4.7uF for the chip as a whole.2013-10-09 2:09 AM
Thank you so much!!