2015-10-08 04:18 AM
Hi,
in this part of theDMA-SetConfig()
function the comments are wrong./*
Memory to Peripheral
*/ if((hdma->Init.Direction) == DMA_MEMORY_TO_PERIPH) { /* Configure DMA Stream destination address */ hdma->Instance->PAR = DstAddress; /* Configure DMA Stream source address */ hdma->Instance->M0AR = SrcAddress; } /*Peripheral to Memory
*/ else { /* Configure DMA Stream source address */ hdma->Instance->PAR = SrcAddress; /* Configure DMA Stream destination address */ hdma->Instance->M0AR = DstAddress; } }Michael
2015-10-08 07:38 AM
Hi Michael ,
Could you precise in which HAL library you have found the issue. So, we can verify it.-Syrine-2015-10-08 11:20 PM
Hi,
I found it in stm32f4xx_hal_dma.cstatic void DMA_SetConfig(DMA_HandleTypeDef *hdma, uint32_t SrcAddress, uint32_t DstAddress, uint32_t DataLength)
{ /* Clear DBM bit */ hdma->Instance->CR &= (uint32_t)(~DMA_SxCR_DBM); /* Configure DMA Stream data length */ hdma->Instance->NDTR = DataLength;/* Peripheral to Memory */
if((hdma->Init.Direction) == DMA_MEMORY_TO_PERIPH) { /* Configure DMA Stream destination address */ hdma->Instance->PAR = DstAddress; /* Configure DMA Stream source address */ hdma->Instance->M0AR = SrcAddress; }/* Memory to Peripheral */
else { /* Configure DMA Stream source address */ hdma->Instance->PAR = SrcAddress; /* Configure DMA Stream destination address */ hdma->Instance->M0AR = DstAddress; } } Michael