2015-10-30 6:22 AM
Hi,
I'm having some issue loading my application from the APPLICATION_ADDRESS -Using a STM32F4 Discovery board -As bootloader application I'm using the STM32F4 examplehttp://www.st.com/web/en/catalog/tools/PF257904
-I'm using the bootloader firmware with default APPLICATION_ADDRESS#define APPLICATION_ADDRESS (uint32_t)0x08008000 -When I'm loading the STSW-STM32068 .bin example on my USB-stick, the demo gets loaded and runs like it should.
so far so good..
-Next step is to create a bin file of my own application.
-I used the following settings for my application:
mem.ld file (.map file is updated accordingly):
FLASH (rx) : ORIGIN = 0x08008000, LENGTH = 1024K
system_stm32f4xx.c file:
#define VECT_TAB_OFFSET 0x8000 /*!< Vector Table base offset field.
-Building the .bin file and rename it ''image.bin'' as needed by the bootloader firmware
-According to the LED's the .bin is loaded to the Flash memory correctly. Also checked with a debugger (memory is filled from 0x08008000).
-When I press the USER button the bootloader starts all over again, loading the .bin file from the USB-stick. I would expect that it will jump the loaded application @ 0x08008000
Do I miss something? Why is the bootloader not jumping to the APPLICATION_ADDRESS?
2015-10-30 8:03 AM
No idea.
Can you use a debugger? Step through the transition code to understand why it doesn't work. The memory will no longer be 1024K, but rather 32K less. Make sure you don't have a bogus stack address. Consider 0x2001FFFC2015-10-30 9:52 AM
Hi,
yes, I have a debugger. Make sure you don't have a bogus stack address. Consider 0x2001FFFC What do you exactly mean with a bogus stack address? According to AN3990 the bootloader firmware checks if the user button is pressed after startup, and also checks if there a user vector table available or not. When not; the firmware upgrade application is executed. That's exactly what's happening./* Test if User button on the Discovery kit is pressed */
if (STM_EVAL_PBGetState(BUTTON_USER) == Bit_RESET)
{
/* Check Vector Table: Test if user code is programmed starting from address ''APPLICATION_ADDRESS'' */
if (((*(__IO uint32_t*)APPLICATION_ADDRESS) & 0x2FFE0000 ) == 0x20000000)
{
/* Jump to user application */
JumpAddress = *(__IO uint32_t*) (APPLICATION_ADDRESS + 4);
Jump_To_Application = (pFunction) JumpAddress;
/* Initialize user application's Stack Pointer */
__set_MSP(*(__IO uint32_t*) APPLICATION_ADDRESS);
Jump_To_Application();
}
}
What's the best way to check if the user vector table is available or not?
2015-10-30 11:00 AM
One that fails the primary test before trying to jump to the application image?
Look at the file in a viewer (file manager, hex editor, etc), decode the bytes at the front of the image into the 32-bit words that compose the vector table. Look at the .MAP files Look at a disassembly output.2015-10-30 1:03 PM
One that fails the primary test before trying to jump to the application image?
Yes, that specific test I added some code to check the vector table:/* Check Vector Table: Test if user code is programmed starting from address
''APPLICATION_ADDRESS'' */
StartAddress = ((*(__IO uint32_t*)APPLICATION_ADDRESS) & 0x2FFE0000 );
if (((*(__IO uint32_t*)APPLICATION_ADDRESS) & 0x2FFE0000 ) == 0x20000000)
{
/* Jump to user application */
JumpAddress = *(__IO uint32_t*) (APPLICATION_ADDRESS + 4);
Jump_To_Application = (pFunction) JumpAddress;
/* Initialize user application's Stack Pointer */
__set_MSP(*(__IO uint32_t*) APPLICATION_ADDRESS);
Jump_To_Application();
}
}
When I load the image that comes with the example:
StartAddress = 0x20000000 -> check is valid
When I load my own application image:
StartAddress = 0x20020000 -> check is invalid
So it seems to be related to my vector table. Any idea what needs to be changed?
Just checked the .map file:
0x0000000020020000 __stack = (ORIGIN (RAM) + 0x20000)
0x0000000020020000 _estack = __stack
0x0000000000000400 __Main_Stack_Size = 0x400
Could ''ORIGIN (RAM) + 0x20000'' cause the issue I have?
2015-10-30 2:03 PM
__stack = (ORIGIN (RAM) + 0x1FFFC)
While technically workable 0x20020000 fails the test, the CPU pre-decrements the SP when it pushes a value.
You could change the test.
/public/STe2ecommunities/mcu/Lists/STM32Java/Flat.aspx?RootFolder=https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Java/Bootloader.%20Load%20program%20with%20stack%20on%20CCM&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000F9A0E3A95BA69146A17C2E80209ADC21¤tviews=47
2015-10-30 11:00 PM
Hi,
I made some changes based on the suggested topic;/* Check Vector Table: Test if user code is programmed starting from address
''APPLICATION_ADDRESS'' */
initsp = ((*(__IO uint32_t*)APPLICATION_ADDRESS) & 0x2FFE0000 );
if ( ((initsp & 3) == 0) && ((initsp > 0x20000000) && (initsp <= 0x20020000))) // in regular RAM region 128KB
{
/* Jump to user application */
JumpAddress = *(__IO uint32_t*) (APPLICATION_ADDRESS + 4);
Jump_To_Application = (pFunction) JumpAddress;
/* Initialize user application's Stack Pointer */
__set_MSP(*(__IO uint32_t*) APPLICATION_ADDRESS);
Jump_To_Application();
}
Now it works, and the application is started like it should.
Thanks for your support.
2015-11-09 12:57 PM
Hi,
now I'm facing a new issue. The application is successfully loaded by the bootloader. After a reset the application starts correctly, throwing out some debug characters via UART. After a few characters the application stops. The debugger doesn't show anything strange. When I load the application on a Discovery board without bootloader (changed linker settings and APPLICATION_ADDRESS), the application doesn't stop and works like it should.Can it be related to RAM/heap? Any idea?
2015-11-09 1:19 PM
There should be no hold-over between the loader/app for RAM usage. I'd look at the clocks and what's going on with SystemInit().
And if you use a debugger, where is the app code ending up? It's real hard to debug things with random symptoms.2015-11-10 1:04 PM
Hi,
according to the debugger, the application holds at a _write() function within retarget.c (printing some startup information). The application always stops after printing the same amount of startup characters. So it doesn’t seems to be random.How can clocks/SystemInit cause this kind of issue? Or what could be wrong?
Thanks.