2024-08-09 12:58 AM
Hi
I use STM32U575I-EV.
I want to periodically read data from an external SPI device without CPU.
The SPI device will emit a data ready signal(active low gpio), so I want to use that as a trigger to read the data.
Ideally, I would like to perform multiple SPI receptions while keeping the CPU in Stop mode.
To read data from a SPI device, just do something like HAL_SPI_Receive_DMA().
Are there any good example projects ?
Or how can I do this ?
I read this articles, but it didn't solve my problem.
Solved: STM32U5 SPI Continuous Communication - STMicroelectronics Community
Best regards.
2024-08-09 7:57 AM
Hi @DK3 ,
I believe that the LPBAM is the good solution for your case.
To know more about the LPBAM, please refer to the wiki article Getting started with LPBAM.
As stated there, a typical example is provided in STM32Cube\Repository\STM32Cube_FW_U5\Projects\NUCLEO-U575ZI-Q\Applications\LPBAM\LPBAM_SPI_TransmitReceive. You can check the readme file to understand more the example.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-08-13 2:37 AM - edited 2024-08-13 2:48 AM
Hi, @Amel NASRI
Thanks to your advices, I was able to do SPI read automatically.
I want to generate a DMA interrupt once every two times and use the receive buffer continuously.
(e.g. Receive1 uses RxBuff[0] ~ RxBuff[7], Receive2 uses RxBuff[8] ~ RxBuff[15])
So, I created two SPI_Receives as shown in the attached image and configured "Transfer Event Generation" as follows.
Receive1 : Transfer Event Generation = TC and HT generated on the last linked-list item
Receive2 : Transfer Event Generation = TC and HT generated on each block
This worked as intended.
Is this setting correct ? Is there a better way ?
When I set Transfer Event Generation of Receive1 and Receive2 to TC and HT generated on the last linked-list item, DMA interrupt was not generated.
The latter setting seemed like the correct setting, but it didn't work.
Please tell me that reason.
Best regards.