2017-06-27 3:54 AM
I recently bought a X-NUCLEO-IDB04A1 and wanted to use it with Arduino. How do I go about it ? Please help me out.
My aim is to collect the sensor data from
http://www.st.com/en/ecosystems/x-nucleo-iks01a1.html
and send it to Arduino pins and transmit the data viaX-NUCLEO-IDB04A1 to another Arduino microcontrollers. I need help to interface X-NUCLEO-IDB04A1 with Arduino.
2017-06-27 4:34 AM
Be careful about IO levels: if you are using Arduino UNO or similar board at 5V, you will need to use level shifters as the BlueNRG chip is not 5V tolerant:
2017-06-29 5:21 AM
Thanks David. I am okay with the voltage values.
I assume that the communication between X-NUCLEO-IDB04A1 and Arduino is SPI. I actually want to know how to send data from Arduino to X-NUCLEO-IDB04A1.
Please help me.