cancel
Showing results for 
Search instead for 
Did you mean: 

Apple USB-C to USB-A Adapter doesn’t work with ST-LINK

alw
Senior
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

Hi Amel NASRI

Yes, when I use a bus-powered USB hub in-between the Apple USB adapter and the STM32 NUCLEO board, the download works ok.

Kind regards,

Al

 

View solution in original post

2 REPLIES 2
Amel NASRI
ST Employee

Hi @alw,

Does using the USB hub resolve the issue for you as suggested in the other discussion?

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hi Amel NASRI

Yes, when I use a bus-powered USB hub in-between the Apple USB adapter and the STM32 NUCLEO board, the download works ok.

Kind regards,

Al