cancel
Showing results for 
Search instead for 
Did you mean: 

Analog watchdog not working the second time.

thebooney
Associate II
Posted on March 28, 2012 at 16:12

I'm having some difficulty with getting the analog watchdog to work a second time. I am able to use it the first time correctly, but I think I might be missing something either when I disable it, or re-enable it because as soon as I start up the AWD the second time, the interrupt fires immediately even though the current ADC value no where near the AWD range I am specifying.

Startup code (Most of the time I do a single ADC read so we default to that):


/* Initialize ADC defaults */

adc_init_def.ADC_Mode = ADC_Mode_Independent;

adc_init_def.ADC_ScanConvMode = DISABLE;

adc_init_def.ADC_ContinuousConvMode = DISABLE;

adc_init_def.ADC_ExternalTrigConv = ADC_ExternalTrigConv_None

adc_init_def.ADC_DataAlign = ADC_DataAlign_Right;

adc_init_def.ADC_NbrOfChannel = 1;


/* Reset the ADC */

ADC_DeInit(adc);


/* Init the ADC */

ADC_Init(adc, &adc_init_def);


/* Enable the ADC */

ADC_Cmd(adc, ENABLE);


/* Calibrate the ADC */

ADC_ResetCalibration(adc);

while
(ADC_GetResetCalibrationStatus(adc)) { }

ADC_StartCalibration(adc);

while
(ADC_GetCalibrationStatus(adc)) { }

When I call the AWD function to set it up, I do the following:


/* Set the mode to continous */

adc_init_def.ADC_ContinuousConvMode = ENABLE;


/* Initialize the ADC again to enable continuous conversion mode */

ADC_DeInit(adc);

ADC_Init(adc, &adc_init_def);


/* Configure the channel */

ADC_RegularChannelConfig(adc, adc_channel, 1, ADC_SampleTime_41Cycles5);


/* Set the watchdog thresholds */

ADC_ClearFlag(adc, ADC_FLAG_AWD);

ADC_AnalogWatchdogThresholdsConfig(adc, current_pos, future_pos);


/* Set the configuration for the watchdog channel */

ADC_AnalogWatchdogSingleChannelConfig(adc, adc_channel);

ADC_AnalogWatchdogCmd(adc, ADC_AnalogWatchdog_SingleRegEnable);


/* Enable the analog watchdog interrupt then enable the interrupts */

ADC_ITConfig(adc, ADC_IT_AWD, ENABLE);


/* Turn on the ADC if its not already on */

ADC_Cmd(adc, ENABLE);


/* Calibrate the ADC */

ADC_ResetCalibration(adc);

while
(ADC_GetResetCalibrationStatus(adc));

ADC_StartCalibration(adc);

while
(ADC_GetCalibrationStatus(adc));

And I handle the AWD inside the ISR as follows:


/* Analog watchdog interrupt */

if
(ADC_GetITStatus(adc, ADC_IT_AWD) != RESET)

{

/* Clear the analog watchdog interrupt flag */

ADC_ClearFlag(adc, ADC_FLAG_AWD);

ADC_ClearITPendingBit(adc, ADC_IT_AWD);

ADC_ITConfig(adc, ADC_IT_AWD, DISABLE);


/* Call the ISR function */

awd_isr->ISR();


/* Disable continous conversion mode, and the watchdog status/owner */

adc_init_def.ADC_ContinuousConvMode = DISABLE;


/* Re-initialize the ADC with continous conversion mode disabled */

ADC_DeInit(adc);

ADC_Init(adc, &adc_init_def);

}

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
thebooney
Associate II
Posted on March 28, 2012 at 16:17

Whoops, last line of the AWD setup should have:

1.
ADC_SoftwareStartConvCmd(adc, ENABLE);

thebooney
Associate II
Posted on March 28, 2012 at 19:18

Scratch that. Turns out my problem was related to power being removed from the potentiometer before I was reading it the second time.