2017-05-23 3:04 AM
Hello,
I have a problem in getting the ti AFE4300 start the ADC measurement. I started with a new board that was designed using reference design on TI. Am trying to communicate with the board through an stm32f103rb(nucleo).
I was set up spi mode 1 and want to use body composition measurement (BCM).
I give 1mHz to afe 4300 board by arm pwm signal.
These are what has happened
1. I can not read ADC data result register. when i read ADC data result, it just show only '0'.
2. the RDY pin status unchanged. it keep high status.
int main()
{ SystemInit(); UART2_Init(); DelayInit(); PWM_Init(); RESET_init(); init_spi1(); resetAFE4300(); initAFE4300(); initBCM();//
while(1) { if(GPIO_ReadInputDataBit(GPIOC,PIN_DRDY) == 1){printf('register_Name\n\r');
printf('0x%X\n\r',readRegister(ADC_DATA_RESULT)); printf('0x%X\n\r',readRegister(ADC_CONTROL_REGISTER)); printf('0x%X\n\r',readRegister(MISC1_REGISTER)); printf('0x%X\n\r',readRegister(MISC2_REGISTER)); printf('0x%X\n\r',readRegister(DEVICE_CONTROL_1)); printf('0x%X\n\r',readRegister(ISW_MATRIX)); printf('0x%X\n\r',readRegister(VSW_MATRIX)); printf('0x%X\n\r',readRegister(IQ_MODE_ENABLE)); printf('0x%X\n\r',readRegister(WEIGHT_SCALE_CONTROL)); printf('0x%X\n\r',readRegister(BCM_DAC_FREQ)); printf('0x%X\n\r',readRegister(DEVICE_CONTROL_2)); printf('0x%X\n\r',readRegister(ADC_CONTROL_REGISTER_2)); printf('0x%X\n\r',readRegister(MISC3_REGISTER));}
else if(GPIO_ReadInputDataBit(GPIOC,PIN_DRDY) == 0){ //printf('%0x\n\r',readRegister(ADC_DATA_RESULT)); printf('low\n\r'); } DelayMs(100); }}void RESET_init(void){
GPIO_InitTypeDef GPIO_InitStructure; //GPIO_PinRemapConfig(GPIO_Remap_SWJ_NoJTRST, ENABLE); //GPIO_PinRemapConfig(GPIO_Remap_SWJ_JTAGDisable, ENABLE); /* Enable the GPIO Clock */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA, ENABLE); RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOC, ENABLE);/* Configure the GPIO pin */
GPIO_InitStructure.GPIO_Pin = PIN_RESET; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOC, &GPIO_InitStructure); GPIO_InitStructure.GPIO_Pin = SPI_CS_PIN; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOA, &GPIO_InitStructure); GPIO_InitStructure.GPIO_Pin = PIN_DRDY; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IPD; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOC, &GPIO_InitStructure); // GPIO_SetBits(GPIOA, GPIO_Pin_4); }uint32_t RDY_read(void){
return GPIO_ReadInputDataBit(GPIOC,PIN_DRDY);}void RESET_HIGH(void){
//GPIOA->BSRR = PIN_RESET; GPIO_SetBits(GPIOC,PIN_RESET);}void RESET_LOW(void){
//GPIOA->BRR = PIN_RESET; GPIO_ResetBits(GPIOC,PIN_RESET);}void resetAFE4300(void){
RESET_LOW(); //printf('111'); DelayMs(100); RESET_HIGH();}void init_spi1(void){ // for MASTER mode GPIO_InitTypeDef GPIO_InitStructure; SPI_InitTypeDef SPI_InitStructure; // GPIO_StructInit (& GPIO_InitStructure); // SPI_StructInit (& SPI_InitStructure);/* Enable GPIOs clock */
RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA, ENABLE); /* Enable SPI clock */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_SPI1, ENABLE);/* Configure SPI SCK pin */
GPIO_InitStructure.GPIO_Pin = SPI_SCK_PIN | SPI_MOSI_PIN | SPI_MISO_PIN; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOA, &GPIO_InitStructure); /* SPI configuration -------------------------------------------------------*/SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex;
SPI_InitStructure.SPI_Mode = SPI_Mode_Master; SPI_InitStructure.SPI_DataSize = SPI_DataSize_8b; SPI_InitStructure.SPI_CPOL = SPI_CPOL_Low; SPI_InitStructure.SPI_CPHA = SPI_CPHA_2Edge; SPI_InitStructure.SPI_NSS = SPI_NSS_Soft;SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_32; //32
SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB; SPI_InitStructure.SPI_CRCPolynomial = 7; SPI_Init(SPI1, &SPI_InitStructure);/* Enable SPI */
SPI_Cmd(SPI1, ENABLE); }void writeRegister(unsigned char address, unsigned int data){
unsigned char firstByte = (unsigned char)(data >> 8); unsigned char secondByte = (unsigned char)data; GPIO_ResetBits(GPIOA, GPIO_Pin_4); SPI_SendByte(address); SPI_SendByte(firstByte); SPI_SendByte(secondByte); GPIO_SetBits(GPIOA, GPIO_Pin_4);}int readRegister(unsigned char address){
int spiReceive = 0; uint8_t spiReceiveFirst = 0; uint8_t spiReceiveSecond = 0;address = address & 0x1F; //Last 5 bits specify address
address = address | 0x20; //First 3 bits need to be 001 for read opcode GPIO_ResetBits(GPIOA, GPIO_Pin_4); SPI_SendByte(address); spiReceiveFirst = SPI_SendByte(0x00); spiReceiveSecond = SPI_SendByte(0x00); GPIO_SetBits(GPIOA, GPIO_Pin_4); spiReceive = (spiReceiveFirst << 8); spiReceive |= spiReceiveSecond; return spiReceive;}void initAFE4300(void){ writeRegister(ADC_CONTROL_REGISTER,0x5140); writeRegister(MISC1_REGISTER,0x0000); // writeRegister(MISC2_REGISTER,0xFFFF); // writeRegister(DEVICE_CONTROL_1,0x0004); //Power down both signal chains writeRegister(ISW_MATRIX,0x0000); writeRegister(VSW_MATRIX,0x0000); writeRegister(IQ_MODE_ENABLE,0x0000); // writeRegister(WEIGHT_SCALE_CONTROL,0x0000); writeRegister(BCM_DAC_FREQ,0x0040); // writeRegister(DEVICE_CONTROL_2,0x0000); writeRegister(ADC_CONTROL_REGISTER_2,0x0011); writeRegister(MISC3_REGISTER,0x00C0);}void initBCM(void)
{ writeRegister(ADC_CONTROL_REGISTER,0x4120); //Differential measurement mode, 32 SPS //4120//C1A0 writeRegister(DEVICE_CONTROL_1,0x0006); //Power up BCM signal chain writeRegister(ISW_MATRIX,0x0408); //Channels IOUTP1 and IOUTN0 writeRegister(VSW_MATRIX,0x0408); //Channels VSENSEP1 and VSENSEN0 writeRegister(ADC_CONTROL_REGISTER_2,0x0063); //ADC selects output of BCM-I output writeRegister(WEIGHT_SCALE_CONTROL,0x0000); //Gain = 1 DAC Offset = 0 0x603F writeRegister(BCM_DAC_FREQ,0x0032); writeRegister(MISC3_REGISTER,0x0030);}uint8_t SPI_SendByte(uint8_t Data)
{ while (SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_TXE) == RESET); SPI_I2S_SendData(SPI1, Data); while (SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_RXNE) == RESET);return SPI_I2S_ReceiveData(SPI1);
}Any leads would be of great help
Regards,
DJ
#afe4300 #stm32f1032018-01-10 12:23 PM
I have exactly the same problem with afe4300 and stm32f100C8T6 microcontroller. Did you managed to solve this problem?
2018-09-20 4:33 AM
Can You send me your code and Schematic ,i will check
rohitpatil597@gmail.com
2019-08-11 12:54 AM
Hi, same problem here ... did anybody figure out what the problem is?