2012-01-13 1:23 AM
Hi,
I want to read all the datas of the Flash Memory on STM32F103RB// Adress start value = 0x08000000 ,end value = 0x0801FFFF;while(Adress != 0x0801FFF) { FLASH_Unlock(); Data=*((uint16_t *) Adres); //read at 0x08000000 flash memory address FLASH_Lock(); Adres=Adres+2; USART_SendData(USART2,Data); }When this program runs, Adress data turns decimal type and i can't see the values .What can i do for describing Adress's data type to increasing hexadecimal type ?2012-01-13 3:06 AM
In the linker script:
MEMORY
{
RAM_C (xrw) : ORIGIN = 0x10000000, LENGTH = 64K
RAM_D (xrw) : ORIGIN = 0x20000000, LENGTH = 128K
FLASH (rx) : ORIGIN = 0x8000000, LENGTH = 1024K
}
2012-01-13 3:21 AM
I tried to say how can i define the adress value and increase it.
I have a for loop and the adress value is increase in the loop, thus i can get the values on all of the adresses in flash memory ?When i define ''u32 Adress=0x08000000;'' or ''uint32_t Adress'' or ''uint64_t Adress;'' this returns me decimal values and i dont want this,i want to debug with hexadecimal form. Can you read the source code and give me advice about this ?2012-01-13 3:24 AM
for(i=0;i<65536;i++) {
FLASH_Unlock(); Data=*((uint16_t *) Adress); //read at Adress^s value flash memory address FLASH_Lock(); Adress=Adress+2; USART_SendData(USART2,Data); }I have the problem at this loop and Adress increasing problem.2012-01-13 3:32 AM
a) You don't need to Lock/Unlock the flash memory to read it
b) USART_SendData is not going to consume 16-bit words c) You need to check the TXE status of the USART before sending each byte d) Your terminal address is wrong// Address start value = 0x08000000 ,end value = 0x0801FFFF;
uint16_t Data;
uint32_t Address;
Address = 0x08000000;
while(Address < 0x0801FFFF) // 512KB limit
{
Data= *((uint16_t *)Address); //read at 0x08000000+ flash memory address
Address += 2;
while(USART_GetFlagStatus(USART2, USART_FLAG_TXE) == RESET);
USART_SendData(USART2,((Data >> 0) & 0xFF)); // Send Low Byte
while(USART_GetFlagStatus(USART2, USART_FLAG_TXE) == RESET);
USART_SendData(USART2,((Data >> 8) & 0xFF)); // Send High Byte
}
This will send the data as raw 8-bit bytes. Plus it will probably overflow the console, and get some corruption. Usually you'd send it in small blocks, with a checksum.
Want the data in hex digits, then you're going to need to break the bytes down into ASCII hex/alpha characters. Want pretty formatting, you'll need to add the code to do that.
void SendHexByte(uint16_t Data)
{
static const char Hex[]=''0123456789ABCDEF'';
while(USART_GetFlagStatus(USART2, USART_FLAG_TXE) == RESET);
USART_SendData(USART2,(Hex[(Data >> 4) & 0xF)]); // Send High Nibble
while(USART_GetFlagStatus(USART2, USART_FLAG_TXE) == RESET);
USART_SendData(USART2,(Hex[(Data >> 0) & 0xF)]); // Send Low Nibble
}
void DumpFlash(void)
{
uint16_t Data;
uint32_t Address;
for(Address = 0x08000000; Address<
0x08020000
; Address += 2)
{
Data= *((uint16_t *)Address); //read at 0x08000000+ flash memory address
SendHexByte(((Data >> 0) & 0xFF)); // Send Low Byte
SendHexByte(((Data >> 8) & 0xFF)); // Send High Byte
}
}
2012-01-13 4:59 AM
I solved this problem thanks to you ..
Thanks clive1 !!!!!2012-01-15 11:51 PM
clive1
your code helped me,thanks a lot again . I'll ask you a question againI want to see these adresses and datas like ->0x08000000 0x07CE0x08000002 0xFFFF.. ........0x0801FFFF 0xFFFFon the hyper terminal screenAdress value is 32-bit so I can't write the algorithm or code for this.Can u help me about it ?How can we send Adress's value2012-01-16 5:46 AM
void SendChar(char Data)
{
while(USART_GetFlagStatus(USART2, USART_FLAG_TXE) == RESET);
USART_SendData(USART2, Data);
}
void SendHexByte(uint16_t Data)
{
static const char Hex[]=''0123456789ABCDEF'';
SendChar(Hex[((Data >> 4) & 0xF])); // Send High Nibble
SendChar(Hex[((Data >> 0) & 0xF)]); // Send Low Nibble
}
void SendHexWord(uint16t Data)
{
SendHexByte(((Data >> 8) & 0xFF)); // Send High Byte
SendHexByte(((Data >> 0) & 0xFF)); // Send Low Byte
}
void SendHexDword(uint32t Data)
{
SendHexWord((uint16_t)((Data >> 16) & 0xFFFF)); // Send High Word
SendHexWord((uint16_t)((Data >> 0) & 0xFFFF)); // Send Low Word
}
void DumpFlash(void)
{
uint16_t Data;
uint32_t Address;
for(Address = 0x08000000; Address<0x08020000; Address += 2)
{
Data= *((uint16_t *)Address); //read at 0x08000000+ flash memory address
SendChar('0')
SendChar('x')
SendHexDword(Address);
SendChar(' ')
SendChar('0')
SendChar('x')
SendHexWord(Data);
SendChar('
');
SendChar('
');
}
}