cancel
Showing results for 
Search instead for 
Did you mean: 

Additional changes for STM32L4 Discovery board as USB host

Mackay.Susan
Associate III
Posted on January 28, 2016 at 03:49

I have an STM32L4 Discovery board that I'm trying to use as a USB host.

Looking at the schematics, I can see the EMIF02-USB03F2 device that is used in conjunction with the USB lines, but it would appear to me that the PD1 and PD2 (that are connected with the pull-down resistors that indicate that this is a USB 'host') are not connected.

Is the schematic correct? If so are we supposed to make any hardware corrections to add the pull-downs?

Also I can't get the Vbus to power up (at least as evidenced by the green LED6 lighting up) UNLESS I set the pin PC9 to be a digital output with a '0' value (which of course is then not controlled by the USB firmware). As this needs to be powered (so that a high-speed device can pull-up the D+ line), is there a bug in the firmware in the STMCubeMX libraries?

Finally, I'm ultimately wanting to use the USB host port for some headphones for audio in and out. I can see some references to sending audio out through the USB connector, but is there an example somewhere is using it as an audio input?

Susan
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0