Question
ADC Reading
Posted on December 06, 2012 at 13:55
Hello All,
I using stm32f2xx. I wanted some help in programing ADC. It might be a silly question. But m a newbei I have to read sensors ouput from ADC123_IN1and ADC123_IN2,ADC12_IN14,ADC12_IN15 of ADC chanells. I have set ADC in scanning mode and I am using DMA. I have set the ranks for all the above channels accordingly. My doubt is when the conversion is completed it will be stored in buffer defined for DMA. So how can i differentiate between the sensor ouput ? Or how will these values from different ADC channels stored in DMA buffer.Any help would be appreciated. Thanks #stm32-adc