2016-01-27 9:55 AM
Hi,
I do have some strange behavior with an ADC, that I cannot explain. I want an ADC to run with a frequency higher than 2 MHz and DMA. I am using an STM32F4 Discovery board, so the ADC's support 2,4MSPS. My configuration is as follows: ABP2: 86 MHz ADC3-Prescaler: 4 Resolution: 6 Bit Sampling Time: 3 Cycles With this configuration, I expect a sampling frequency of ~2,4MHz (86/4/(6+3)). I want to verify it by using a pin, that I toggle on the DMA callbacks (half-full and full). My DMA memory size is set to 160 values. Unfortunately the pin does not toggle. When reducing the sampling frequency to ~1,2 MHz by setting the ADC prescaler to 8, I get an pulse signal at the pin with ~7,5kHz. This is axactly the freqeuncy I expected (7,5kHz*160samples = 1,2MSPS) So sampling with 1,2 MSPS works but with higher freqeuncies does not. Even setting the adc prescaler to 6, does not work. :( What am I missing? I would expect, that this s hould work. T2016-01-27 11:10 PM
This is my ADC configuration:
hadc3.Instance = ADC3;
hadc3.Init.ClockPrescaler = ADC_CLOCKPRESCALER_PCLK_DIV4; hadc3.Init.Resolution = ADC_RESOLUTION6b; hadc3.Init.ScanConvMode = ENABLE; hadc3.Init.ContinuousConvMode = ENABLE; hadc3.Init.DiscontinuousConvMode = DISABLE; hadc3.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE; hadc3.Init.DataAlign = ADC_DATAALIGN_RIGHT; hadc3.Init.NbrOfConversion = 1; hadc3.Init.DMAContinuousRequests = ENABLE; hadc3.Init.EOCSelection = EOC_SINGLE_CONV; HAL_ADC_Init(&hadc3); sConfig.Channel = ADC_CHANNEL_0; sConfig.Rank = 1; sConfig.SamplingTime = ADC_SAMPLETIME_3CYCLES; HAL_ADC_ConfigChannel(&hadc3, &sConfig); My DMA initialization looks like this:hdma_adc3.Instance = DMA2_Stream1;
hdma_adc3.Init.Channel = DMA_CHANNEL_2; hdma_adc3.Init.Direction = DMA_PERIPH_TO_MEMORY; hdma_adc3.Init.PeriphInc = DMA_PINC_DISABLE; hdma_adc3.Init.MemInc = DMA_MINC_ENABLE; hdma_adc3.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE; hdma_adc3.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE; hdma_adc3.Init.Mode = DMA_CIRCULAR; hdma_adc3.Init.Priority = DMA_PRIORITY_LOW; hdma_adc3.Init.FIFOMode = DMA_FIFOMODE_DISABLE; hdma_adc3.Init.MemBurst = DMA_MBURST_SINGLE; hdma_adc3.Init.PeriphBurst = DMA_PBURST_SINGLE; HAL_DMA_Init(&hdma_adc3);__HAL_LINKDMA(hadc,DMA_Handle,hdma_adc3);
2016-02-01 8:12 AM
In another attempt, I have setup my STM32F429I-Discovery board as described in
http://www.st.com/web/en/resource/technical/document/application_note/DM00050879.pdf
. Clock source: external clock (8 MHz) provided by a generator, PLL is enabled, fCPU = 144 MHz ... with fADC = 36 MHz, sampling time = 3 ADC cycles and ADC resolution = 12 bits in order to achieve the fastest ADC conversion (2.4 Msps). DMA is activated and a pin is toggled on the callbacks (half-full and full). In this configuration it does not work, too :( Only, when I decrease the sampling rate to 1.2 Msps the pin toggles. I doubt, that the DMA limits the ADC. Or am I wrong with this assumption?2016-02-02 2:17 AM
I have tried the same settings on my STM32F746G-DISCO and its works as expected. I have also tried another STM32F429I-DISCO, but it does not work too.
I would really like to understand how to get the ADC of STM32F4 working with 2.4Msps. I hope anyone can help or provide some working example code.