cancel
Showing results for 
Search instead for 
Did you mean: 

ADC in STM32F4 Discovery

its
Associate II
Posted on January 02, 2013 at 08:06

hi:

    i found that ADC12 and ADC123 in STM32F4 Discovery.  How Can I use them?

   or whats the way to use ADC on STM32F4Discovery? I have library of STM32F4xx.c in that ADC1, ADC2, ADC3 are only defined? which are not in LQFP100 pakage as i found, i think I have ADC12 and ADC123

how can I use them and waht abt there base addresses?

#adc
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
crt2
Associate II
Posted on January 02, 2013 at 13:19

ADC= analog-digital Converter. You can use different ADCs (and different channels) with different pins. In datasheet at pins it writes ADC12 or ADC123 but that only means that that pin can be used with either ADC1 or ADC2 and in last case in any 3 of them. You also have channel beside that (IN) which connects you pin-to adc channel.