cancel
Showing results for 
Search instead for 
Did you mean: 

Abnormal operation after reset (BOOT0)

Jae Bong
Associate
Posted on August 29, 2017 at 06:37

STM32F103RC Abnormal symptom occurred while using Help request.

Resetting without a ground connection to the BOOT0 pin will result in some products not booting.

If this problem occurred from the beginning of development, it would have used to connect to ground. But I have been using it for 3 years now, it is frustrating because I have problems now.

Question 1: Why? Is there a product that boots after a reset, and a product that does not boot?

Question 2: Why? Is this problem only in recent products?

And I do not use the boot loader area

The problem is that the current BOOT0 pin can not be connected to ground

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
David SIORPAES
ST Employee
Posted on August 29, 2017 at 12:56

BOOT0 pin must be properly hooked to ground if you want to avoid booting from System Memory. It cannot be left floating.

Please refer to AN2586, page 15 and 24.