Skip to main content
jones.david
Associate III
July 22, 2015
Question

a little help

  • July 22, 2015
  • 0 replies
  • 425 views
Posted on July 22, 2015 at 23:06

i ran freertos + lwip (MII) with mxcube in stm32f407

sorry i did not previous Post ans simply i'll tell you my experiences

1. be careful about Gpio Pin Initializes check your schematic with your cube Settings

2. you should maintain this condition on cube. there is good example in the cube folder in Project/Stm32f40G/Application/Lwip/ (there is just a folder with freerotos)

(this address is what i remember but it's almost correct)

in that project there is 2 header files with names of ''lwipopts.h'' and ''opts.h''

make all of mxcube parameter the same with this two header files

3.this step is very important.you should add this line to your code in ''lwipopts.h'' user Code at the end of file

''#define LWIP_COMPAT_MUTEX 1

and enable using mutex in freertos settings

4. in freertos settings by default you have 7 prioritis in tasks

you should be careful not to increase thread_tcp_Prio more than this value or else you should increase your freertos priorities

5. create power down external interrupt like the example

6. u can use the example procedure to create your own project

hope this help you
    This topic has been closed for replies.