cancel
Showing results for 
Search instead for 
Did you mean: 

5V & 3V3 POWER SUPPLY BAT60 DIODES: are they critical ?

jean_prieur
Associate III
Posted on May 20, 2013 at 12:11

Hello,

I'm currently designing my own schematic based on the STM32F4DISCOVERY board.

The two BAT60 power supply protection diodes (D1 & D3) are not relevant for me because they generate a dropout voltage: +5V is in fact +4.7V and +3.3V is +3V.

I want a full +5V to supply my analog functions (based on opamps) and a full +3.3V to allow the STM32F407 to generate/convert 3.3V signals with the DAC/ADC. (my only board power supply is the USB VBUS)

Are the BAT60 really critical concerning the USB power supply protection ? I need to remove them...

Thanks !
This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
raptorhal2
Lead
Posted on May 20, 2013 at 15:07

Without the diodes, it is up to your design to ensure that the USB does not see more than 5V and the F4 does not see more than 3.6 V.

Cheers, Hal

jean_prieur
Associate III
Posted on May 20, 2013 at 17:55

Thanks !

Is there a cheap solution to protect these power supplies from highter voltages, without decreasing the voltage ? For example with zener diodes...

raptorhal2
Lead
Posted on May 21, 2013 at 01:50

Why not use a 3.6V regulator instead of a 3.3V regulator to get the desired ADC range of 3.3V ? Convert internal channel 17 to get the actual reference voltage.

I am puzzled about using 5V for the analog functions. Are you mounting the board on a motherboard with analog amps ?

Cheers, Hal

jean_prieur
Associate III
Posted on May 22, 2013 at 17:05

The 3.6V regulator can be a good solution.

The +5V of the USB is enough for my application (amplifing the analog DAC signals outputs). Yes, I already mounted the discovery board on a motherboard with analog opamps, but now I want to create a single board with the uC and analog part, all powered by the USB 5V, because it's a part of my specifications...

donald2
Associate II
Posted on May 28, 2013 at 08:42

You can implement polarity protection with a MOSFET rather than a diode.

To protect from the positive rail, use a P-channel MOSFET.  Connect the positive input to the drain, the load to the source, and the gate to ground.  This is 'backwards' from the usual configuration.  The device initially conducts because of the body diode.  With higher voltages the gate turns on allowing resistive flow, just as with 'forward' operation.

An N-channel MOSFET could do the same job on the negative power side.  N-channel devices are more efficient (either lower cost or better specs for the same cost), but sometimes a design that disconnects the negative/ground isn't suitable.

Extra low dropout voltage regulators are available.  They are based on MOSFETs rather than bipolar transistors, thus operating with less than the 300mV drop of a saturated bipolar transistor.