cancel
Showing results for 
Search instead for 
Did you mean: 

32F429IDISCOVERY ADC single conversion

mchalapetr
Associate II
Posted on April 27, 2015 at 19:58

Hi,

I am having issue regarding an ADC configuration on 32F429IDISCOVERY board. I have a battery power application where I want to measure the battery voltage. This voltage is above the reference of the board (VCC) so I need to use a voltage divider. The divider is as big as possible to drain as low current as possible in my case combination 1M/330k resistors plus parallel 100n capacitor to the 330k. My idea was to measure voltage with ADC for example once every ten seconds and print id out. I believed that this was enough time to charge the capacitor and then by S&H circuit get the voltage. Problem is that this is not working...

When I connect some voltage for example 2V directly to ADC pin it shows approx. 2V very nicely but when I connect the voltage across the voltage divider the voltage on the divider drops to zero.

So basically the ADC measures good value because there really is zero but why? Why the voltage on the divider drops when I connect it to the ADC pin? I dont know what to do with it...It just must work...Using OPAMP didn't help either...

The code I am using is as follows:

void ADC1_CH1_Init(void){

    GPIO_InitTypeDef GPIO_InitDef;

    ADC_InitTypeDef ADC_InitStruct;

ADC_CommonInitTypeDef ADC_CommonInitStruct;

RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE);

RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1, ENABLE);

    // GPIO config

//                          PA1

GPIO_InitDef.GPIO_Pin = GPIO_Pin_1;

    GPIO_InitDef.GPIO_Mode = GPIO_Mode_AN;

    GPIO_InitDef.GPIO_OType = GPIO_OType_PP;

    GPIO_InitDef.GPIO_PuPd = GPIO_PuPd_NOPULL;

    GPIO_InitDef.GPIO_Speed = GPIO_Speed_100MHz;

    GPIO_Init(GPIOA, &GPIO_InitDef);

    // Set common ADC settings

ADC_CommonInitStruct.ADC_DMAAccessMode = ADC_DMAAccessMode_Disabled;

ADC_CommonInitStruct.ADC_Mode = ADC_Mode_Independent;

ADC_CommonInitStruct.ADC_Prescaler = ADC_Prescaler_Div4;

ADC_CommonInitStruct.ADC_TwoSamplingDelay = ADC_TwoSamplingDelay_5Cycles;

ADC_CommonInit(&ADC_CommonInitStruct);

// Init ADC settings

ADC_InitStruct.ADC_ContinuousConvMode = DISABLE;

ADC_InitStruct.ADC_DataAlign = ADC_DataAlign_Right;

ADC_InitStruct.ADC_ExternalTrigConv = DISABLE;

ADC_InitStruct.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None;

ADC_InitStruct.ADC_NbrOfConversion = 1;

ADC_InitStruct.ADC_ScanConvMode = DISABLE;

ADC_InitStruct.ADC_Resolution = ADC_Resolution_12b;

    ADC_Init(ADC1, &ADC_InitStruct);

ADC_Cmd(ADC1, ENABLE);

}

uint16_t ADC1_CH1_Read(void) {

ADC_RegularChannelConfig(ADC1, ADC_Channel_1, 1, ADC_SampleTime_3Cycles);

// Start software conversion

ADC_SoftwareStartConv(ADC1);

// Wait till done

while(ADC_GetFlagStatus(ADC1,ADC_FLAG_EOC)==RESET);

return ADC_GetConversionValue(ADC1);

}

#adc #stm32f4 #disco
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Posted on April 27, 2015 at 21:24

Check the input impedance of the ADC. Pretty sure the 1M arm of the divider is going to route through the ADC instead

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
raptorhal2
Lead
Posted on April 28, 2015 at 03:44

When you use  an 429 Discovery for analog conversions, you discover either by reading the reference manual or by bitter experience that PA1 is dedicated to LG3D20 interrupt functions on the board. You have 3 choices - PA5, PC3 or PF6.

I wish ST would use a darker shade on the pin allocations table to indicate free I/O.

Cheers, Hal

mchalapetr
Associate II
Posted on April 30, 2015 at 15:12

Thank you very much...I tried more than one pin/channel but to be honest I did not check the wiring...Thanks very very much...