2024-06-10 2:07 AM
How can i add multiple charts to the dashboard? I want to use at least 2-charts in the dashboard, and monitor some variables (not an array) on a chart while some other variables (not an array) on a different chart. I have seen one chart + gauge(s) examples a lot. But all I need is to use two or more charts in the dashboard.
Solved! Go to Solution.
2024-06-10 2:36 AM
Hello
It is possible to have multiple charts.
The flow can either have 2 groups of variable, one for each chart, or one group and then filter the data sent to each chart.
Please, read this wiki page to have more details : How_to_filter_or_route_variables
The examples show one chart and one gauge, but it is also possible to have multiple charts.
I would suggest to use the last example of "3.4. Switch nodes with several conditions", but connect the outputs to different charts.
Best regards
2024-06-10 2:36 AM
Hello
It is possible to have multiple charts.
The flow can either have 2 groups of variable, one for each chart, or one group and then filter the data sent to each chart.
Please, read this wiki page to have more details : How_to_filter_or_route_variables
The examples show one chart and one gauge, but it is also possible to have multiple charts.
I would suggest to use the last example of "3.4. Switch nodes with several conditions", but connect the outputs to different charts.
Best regards
2024-06-10 2:37 AM
Hello,
Is that a TouchGFX subject related?
2024-06-10 3:08 AM
No. It is not TouchGFX related. I am trying to control a Permanent Magnet Synchronous Motor (PMSM).
2024-06-10 3:16 AM - edited 2024-06-10 3:40 AM
Ok then the thread needs to be moved to the correct Forum.
2024-06-10 4:12 AM
Your reply solved my problem. Thanks.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.