2024-08-09 9:54 PM
Hi,
I am prototyping a custom PCB with integrated ESC for a BLDC Motor (Datasheet attached). For this purpose, I plan of using STSPIN32F0 due to versatile options following this article. The article's design is based on 45A max consumption and looking at BLDC's datasheet this seems appropriate. In addition to this, I would like to add following capabilities i.e. Control/ Info through BLE along with BLE DFU.
Please recommend/ suggest, any ST's SiP supporting BLE or war around to accomplish the sample.
Regards