cancel
Showing results for 
Search instead for 
Did you mean: 

STEVAL-CTM01xV1 firmware

PGinhson
Associate III

Hi.
I have the IDE with the STEVAL-CTM01xV1 shunt_FOC and downloaded on the Board. As the example came, the motor doesen't work.

I opened the main.c file and I could see that it does not have any function inside the main while(1) loop. How could I have a working example to start testing the board?

Blessings on your courage, that's the way to the stars
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
GMA
ST Employee

Hello,

Readme.txt is automatically opened once you select the example, I have attached the file in my previous response.

Selecting the monitor mode, you can select the motors and start/stop buttons.

GMA_0-1706770658327.png

 

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA

View solution in original post

4 REPLIES 4
GMA
ST Employee

Hello,

Did you go through readme.txt document?
As mentioned in the readme.txt, for testing "6. Run the example : through the STM32 MC Workbench monitor GUI (Start Motor), or/and by pressing the Start/Stop button."
This example is for a Selni motor.

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA

Thank you, but...

Where is the start/stop button on STEVAL-CTM011V1?

Blessings on your courage, that's the way to the stars

Where is that "readme.txt" document?

Blessings on your courage, that's the way to the stars
GMA
ST Employee

Hello,

Readme.txt is automatically opened once you select the example, I have attached the file in my previous response.

Selecting the monitor mode, you can select the motors and start/stop buttons.

GMA_0-1706770658327.png

 

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA