cancel
Showing results for 
Search instead for 
Did you mean: 

PWM Combined 3 Phase Mode, ADC Trigger, unexpected behaviour

EDuat.1
Associate III

Hi guys,

I am working on Motor Control and I need to set up Combined PWM and ADC trigger syncronize together.Last situation is PWMs working and ADC is trigered so when the ADC is triggered ,interrupt event is running in HAL_ADCEx_InjectedConvCpltCallback that I put in it Led Toggle what I see is trigger event is not runnning in every pwm period.Trigger event is running 1 time and no interrupt 2 times and again running interrupt.If I am gonna tell it in different way --> run wait wait run wait wait run ... Like that ,I am not sure drawing right but probably enough.Also HAL_TIM_TriggerCallback doesn't work.

_____-----_-----_______-----_-----_______-----_-----________-----_-----_______-----_-----___ PWM 1

____-------_-------____-------_-------____-------_-------_____-------_-------____-------_-------___ PWM 2

___--------_--------___--------_--------___--------_--------___--------_--------___--------_-------___ PWM 3

-------------______________________________________________----------------------------------- LED inside interrupt

Codes below

//----------------------- tim.c -----------------------//
#include "tim.h"
 
extern uint32_t timerPeriod;
 
TIM_HandleTypeDef htim1;
 
void MX_TIM1_Init(void)
{
  TIM_ClockConfigTypeDef sClockSourceConfig = {0};
  TIM_MasterConfigTypeDef sMasterConfig = {0};
  TIM_OC_InitTypeDef sConfigOC = {0};
  TIM_BreakDeadTimeConfigTypeDef sBreakDeadTimeConfig = {0};
 
  htim1.Instance = TIM1;
  htim1.Init.Prescaler = 0;
  htim1.Init.CounterMode = TIM_COUNTERMODE_CENTERALIGNED2;
  htim1.Init.Period = timerPeriod;
  htim1.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
  htim1.Init.RepetitionCounter = 0;
  htim1.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
  if (HAL_TIM_Base_Init(&htim1) != HAL_OK)
  {
    Error_Handler();
  }
  sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
  if (HAL_TIM_ConfigClockSource(&htim1, &sClockSourceConfig) != HAL_OK)
  {
    Error_Handler();
  }
  if (HAL_TIM_PWM_Init(&htim1) != HAL_OK)
  {
    Error_Handler();
  }
  sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
  sMasterConfig.MasterOutputTrigger2 = TIM_TRGO2_OC5REF_RISING_OC6REF_FALLING;
  sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_ENABLE;
  if (HAL_TIMEx_MasterConfigSynchronization(&htim1, &sMasterConfig) != HAL_OK)
  {
    Error_Handler();
  }
  sConfigOC.OCMode = TIM_OCMODE_PWM1;
  sConfigOC.Pulse = 0;
  sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;
  sConfigOC.OCNPolarity = TIM_OCNPOLARITY_HIGH;
  sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;
  sConfigOC.OCIdleState = TIM_OCIDLESTATE_RESET;
  sConfigOC.OCNIdleState = TIM_OCNIDLESTATE_RESET;
  if (HAL_TIM_PWM_ConfigChannel(&htim1, &sConfigOC, TIM_CHANNEL_1) != HAL_OK)
  { Error_Handler(); }
  sConfigOC.Pulse = 0;
  if (HAL_TIM_PWM_ConfigChannel(&htim1, &sConfigOC, TIM_CHANNEL_2) != HAL_OK)
  { Error_Handler(); }
  sConfigOC.Pulse = 0;
  if (HAL_TIM_PWM_ConfigChannel(&htim1, &sConfigOC, TIM_CHANNEL_3) != HAL_OK)
  { Error_Handler(); }
  sConfigOC.OCMode = TIM_OCMODE_PWM2;
  sConfigOC.Pulse = 1000;
  if (HAL_TIM_PWM_ConfigChannel(&htim1, &sConfigOC, TIM_CHANNEL_5) != HAL_OK)
  { Error_Handler(); }
  sBreakDeadTimeConfig.OffStateRunMode = TIM_OSSR_DISABLE;
  sBreakDeadTimeConfig.OffStateIDLEMode = TIM_OSSI_DISABLE;
  sBreakDeadTimeConfig.LockLevel = TIM_LOCKLEVEL_OFF;
  sBreakDeadTimeConfig.DeadTime = 200;
  sBreakDeadTimeConfig.BreakState = TIM_BREAK_DISABLE;
  sBreakDeadTimeConfig.BreakPolarity = TIM_BREAKPOLARITY_HIGH;
  sBreakDeadTimeConfig.BreakFilter = 0;
  sBreakDeadTimeConfig.BreakAFMode = TIM_BREAK_AFMODE_INPUT;
  sBreakDeadTimeConfig.Break2State = TIM_BREAK2_DISABLE;
  sBreakDeadTimeConfig.Break2Polarity = TIM_BREAK2POLARITY_HIGH;
  sBreakDeadTimeConfig.Break2Filter = 0;
  sBreakDeadTimeConfig.Break2AFMode = TIM_BREAK_AFMODE_INPUT;
  sBreakDeadTimeConfig.AutomaticOutput = TIM_AUTOMATICOUTPUT_DISABLE;
  if (HAL_TIMEx_ConfigBreakDeadTime(&htim1, &sBreakDeadTimeConfig) != HAL_OK)
  {  Error_Handler(); }
  HAL_TIM_MspPostInit(&htim1);
}
 
void HAL_TIM_Base_MspInit(TIM_HandleTypeDef* tim_baseHandle)
{
  if(tim_baseHandle->Instance==TIM1)
  {
    __HAL_RCC_TIM1_CLK_ENABLE();
    HAL_NVIC_SetPriority(TIM1_UP_TIM16_IRQn, 0, 0);
    HAL_NVIC_EnableIRQ(TIM1_UP_TIM16_IRQn);
    HAL_NVIC_SetPriority(TIM1_TRG_COM_TIM17_IRQn, 0, 0);
    HAL_NVIC_EnableIRQ(TIM1_TRG_COM_TIM17_IRQn);
  }
}
void HAL_TIM_MspPostInit(TIM_HandleTypeDef* timHandle)
{
  GPIO_InitTypeDef GPIO_InitStruct = {0};
  if(timHandle->Instance==TIM1)
  {
    __HAL_RCC_GPIOA_CLK_ENABLE();
    __HAL_RCC_GPIOB_CLK_ENABLE();
    /**TIM1 GPIO Configuration
    PA7     ------> TIM1_CH1N
    PB0     ------> TIM1_CH2N
    PB1     ------> TIM1_CH3N
    PA8     ------> TIM1_CH1
    PA9     ------> TIM1_CH2
    PA10     ------> TIM1_CH3
    */
    GPIO_InitStruct.Pin = PWM_UL_Pin|PWM_UH_Pin|PWM_VH_Pin|PWM_WH_Pin;
    GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
    GPIO_InitStruct.Pull = GPIO_NOPULL;
    GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
    GPIO_InitStruct.Alternate = GPIO_AF6_TIM1;
    HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
 
    GPIO_InitStruct.Pin = PWM_VL_Pin|PWM_WL_Pin;
    GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
    GPIO_InitStruct.Pull = GPIO_NOPULL;
    GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
    GPIO_InitStruct.Alternate = GPIO_AF6_TIM1;
    HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
  }
}
 
//----------------------- main.c -----------------------//
 
int main(void)
{
  HAL_Init();
  SystemClock_Config();
 
  mcuFreq = HAL_RCC_GetSysClockFreq();
  timerPeriod = (uint32_t)((mcuFreq / 10000) - 1);
 
  MX_GPIO_Init();
  MX_TIM1_Init();
  MX_ADC1_Init();
  MX_USART1_UART_Init();
 
  __HAL_UART_FLUSH_DRREGISTER(&huart1);
  __HAL_TIM_ENABLE_IT(&htim1,TIM_IT_TRIGGER | TIM_IT_UPDATE);
 
  if(HAL_ADCEx_Calibration_Start(&hadc1, ADC_SINGLE_ENDED) != HAL_OK); Error_Handler();
   HAL_ADCEx_InjectedStart_IT(&hadc1);
 
  valBuf[0] = setDutyPercentage(40);
  valBuf[1] = setDutyPercentage(50);
  valBuf[2] = setDutyPercentage(80);
 
 if(HAL_TIMEx_GroupChannel5(&htim1, (TIM_GROUPCH5_OC1REFC |\
                                          TIM_GROUPCH5_OC2REFC |\
                                          TIM_GROUPCH5_OC3REFC)) != HAL_OK)	Error_Handler();
  //if(HAL_TIMEx_GroupChannel5(&htim1, TIM_GROUPCH5_OC3REFC) != HAL_OK)	Error_Handler();
 
  if( HAL_TIM_Base_Start(&htim1) != HAL_OK )	Error_Handler();
 
  if(HAL_TIM_PWM_Start_IT(&htim1, TIM_CHANNEL_1) != HAL_OK) 	Error_Handler();
  if(HAL_TIMEx_PWMN_Start_IT(&htim1, TIM_CHANNEL_1) != HAL_OK)	Error_Handler();
  if(HAL_TIM_PWM_Start_IT(&htim1, TIM_CHANNEL_2) != HAL_OK) 	Error_Handler();
  if(HAL_TIMEx_PWMN_Start_IT(&htim1, TIM_CHANNEL_2) != HAL_OK)	Error_Handler();
  if(HAL_TIM_PWM_Start_IT(&htim1, TIM_CHANNEL_3) != HAL_OK) 	Error_Handler();
  if(HAL_TIMEx_PWMN_Start_IT(&htim1, TIM_CHANNEL_3) != HAL_OK)	Error_Handler();
  if(HAL_TIM_PWM_Start_IT(&htim1, TIM_CHANNEL_5) != HAL_OK)		Error_Handler(); //ADC Trigger
 
 
  TIM1->CCR1 = valBuf[0];
  TIM1->CCR2 = valBuf[1];
  TIM1->CCR3 = valBuf[2];
 
  HAL_UART_Receive_IT(&huart1, uartRxBuf, 1);
 
  while (1)
  {
	  u16TimerVal = __HAL_TIM_GET_COUNTER(&htim1);
  }
}
 
void SystemClock_Config(void)
{
  RCC_OscInitTypeDef RCC_OscInitStruct = {0};
  RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
  RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};
 
  HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1_BOOST);
 
  RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
  RCC_OscInitStruct.HSEState = RCC_HSE_ON;
  RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
  RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
  RCC_OscInitStruct.PLL.PLLM = RCC_PLLM_DIV6;
  RCC_OscInitStruct.PLL.PLLN = 85;
  RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
  RCC_OscInitStruct.PLL.PLLQ = RCC_PLLQ_DIV2;
  RCC_OscInitStruct.PLL.PLLR = RCC_PLLR_DIV2;
  if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
  { Error_Handler(); }
 
  RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
                              |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
  RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
  RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
  RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
  RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
 
  if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_4) != HAL_OK)
  {Error_Handler(); }
 
  PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_USART1|RCC_PERIPHCLK_ADC12;
  PeriphClkInit.Usart1ClockSelection = RCC_USART1CLKSOURCE_PCLK2;
  PeriphClkInit.Adc12ClockSelection = RCC_ADC12CLKSOURCE_SYSCLK;
  if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
  {Error_Handler(); }
}
 
uint32_t setDutyPercentage(uint32_t val)
{
	return (( val * (timerPeriod - 1)) / 100);
}
 
void HAL_ADCEx_InjectedConvCpltCallback(ADC_HandleTypeDef *hadc)
{
	ADConvertedValues[2] = HAL_ADCEx_InjectedGetValue(&hadc1, ADC_INJECTED_RANK_3);
	HAL_GPIO_TogglePin(GPIOA,GPIO_PIN_5);
}
 
//This interrupt doesn't work
void HAL_TIM_TriggerCallback(TIM_HandleTypeDef *htim)
{
	//HAL_GPIO_TogglePin(GPIOA,GPIO_PIN_5);
	__HAL_TIM_CLEAR_FLAG(&htim1,TIM_IT_TRIGGER);
}

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
EDuat.1
Associate III

Solved.Because of discontinuous mode

View solution in original post

2 REPLIES 2
EDuat.1
Associate III

Solved.Because of discontinuous mode

Laurent Ca...
Lead II

Dear @Community member​ 

Happy for you.

Feel free to ask any other questions you want.

Best regards

Laurent Ca...