2021-09-16 2:03 AM
I have STM3210B-MCKIT PMSM starter control kit, It is worked through LCD and for start and stop the motor.
but I would like to develop a new controller and change the control system. I would like to a guide and If there is a library that has the projects for this starter kit?
how can I measure the currents with an oscilloscope through ADC, I can find these pins in the kit?
I asked after a spent a long time, so please help me!
2021-10-20 5:28 AM
Dear @ADiab.2
Welcome to the STM32 Community
Sorry for late answer.
Could you give more details to the STM32 Community about your setup -the material you use- ?
(HW and also SW: CPU(s), tools and versions, board(s), motor(s) and so on)
And more especially did you use STM32 MC tools (such as MC_suite, STM32 MC Motor Profile, STM32 MC SDK, STM32 MC Workbench, the used example, the origin of the base of your application source code, and so on)?
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.