cancel
Showing results for 
Search instead for 
Did you mean: 

B-G431B-ESC1 / MCSDK Motor Pilot/Profiler Failed Connection

TH3221
Associate III

Board: B-G431B-ESC1

OS: Windows 11

Attempting to use the Motor Pilot or Profiler but unable to connect. I know I am connected because ST-Link can read the MCU and I am able to program it. From previous posts it seems to be related to the version of MCSDK so I attempted to use 5.4.8, 6.2.1, 6.2.0, 6.1.0, and 6.3.1. Done the obvious restart computer, board, run as admin.

  • Generated Firmware using the MC workbench, ensured Motor Profiler was checked in Application Configuration and uploaded to board
  • Double checked to make sure UART was initialized
  • Another post said to set build configuration to release, didnt work

 

Not sure how to diagnose from here 

 

From the Motor Profiler (Any of them)

[INFO] - UART worker: Successfully open port COM6 @ 115200

[INFO] - : try to configure the board'

From the Motor Profiler (Any of them)

[ERROR] - : Failed to discover Board at 1843200 Bauds and 115200 Bauds

[INFO] - : disconnect UART START

[INFO] - : Disconnected from board

[INFO] - : disconnect UART END

More information from the programmer

11:54:11 : ST-LINK SN : 0674FF485051727187183257
11:54:11 : ST-LINK FW : V2J45M30
11:54:11 : Board : B-G431B-ESC1
11:54:11 : Voltage : 3.23V
11:54:11 : SWD freq : 4000 KHz
11:54:11 : Connect mode: Normal
11:54:11 : Reset mode : Software reset
11:54:11 : Device ID : 0x468
11:54:11 : Revision ID : Rev X
11:54:11 : ST-LINK SN : 0674FF485051727187183257
11:54:11 : ST-LINK FW : V2J45M30

11 REPLIES 11
shorai
Associate III

I've just had the same problem.

Appears to be fixed with an upgrade of the firmware and download of the example program.

i.e.  - ST-Link needs to be updated to latest

       - Install a dummy version of your project using parameters any motor

        - The run the profiler and get updated profile for your motor.

Hope thay helps 

Kamil1
Associate III

Hi, I have exactly the same issue. Is there any clear solution to this?

I'm using the MCSDK 6.4.1, motor pilot 6.4.1, and stlink firmware is V2J47M34

 

Thank you