2014-07-30 6:16 AM
Hi,
I'm trying to initialize a usart, and read some data on a Terminal. The terminal receives some data but not the good one. The problem seems to be a clock problem, and the usart register BRR looks wrong. Moreover, in the terminal settings, it reeds the rated speed at 115200 instead of 57600 and even if i change the baudrate in the usart init, the terminal still read 115200. Any idea what could be the problem ? Thanks #stm32f105 #stm32f105-usb-host2014-07-30 7:26 AM
It looks wrong, but you can't tell us what it is?
It should be a function of the APBx clock the USART is attached too. The BRR might be wrong if the HSE_VALUE doesn't match the external crystal on the board, or related PLL settings. The terminal program will just tell you what you selected as a baud rate for the COM port. Have the STM32 send a repetitive stream of data, say 'U' or 0x55, get a SCOPE, and MEASURE the bit timings. If these appear wrong, step back and look at the clocks being supplied to the part, and output internal clocks via MCOx pins, and MEASURE those. For a 36 MHz APB clock I'd expect BRR for a 115200 baud clock to be 312 or 3132014-07-30 7:58 AM
Thanks for the answer,
here is the code : #define UART_USER USART2 #define USART_USER_TB_TX GPIO_Pin_2 #define USART_USER_TB_PIN_SOURCE_TX GPIO_PinSource2 #define USART_USER_TB_RX GPIO_Pin_3 #define USART_USER_TB_PIN_SOURCE_RX GPIO_PinSource3 #define USART_USER_TB_GPIO_PORT GPIOA #define PERIF_CLOCK_USART_TB_USER RCC_APB1Periph_USART2 #define PERIF_CLOCK_PINS_USART_TB_USER RCC_APB2Periph_GPIOA void uart_init_user() { GPIO_InitTypeDef GPIO_InitStruct; // this is for the GPIO pins used as TX and RX USART_InitTypeDef USART_InitStruct; // this is for the USART1 initilization NVIC_InitTypeDef NVIC_InitStructure; // this is used to configure the NVIC (nested vector interrupt controller) RCC_APB1PeriphClockCmd(PERIF_CLOCK_USART_TB_USER, ENABLE); RCC_APB2PeriphClockCmd(PERIF_CLOCK_PINS_USART_TB_USER, ENABLE); GPIO_InitStruct.GPIO_Pin = USART_USER_TB_TX; GPIO_InitStruct.GPIO_Mode = GPIO_Mode_AF_PP; // the pins are configured as alternate function so the USART peripheral has access to them GPIO_InitStruct.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(USART_USER_TB_GPIO_PORT, &GPIO_InitStruct); GPIO_InitStruct.GPIO_Pin = USART_USER_TB_RX; GPIO_InitStruct.GPIO_Mode = GPIO_Mode_IN_FLOATING; GPIO_Init(USART_USER_TB_GPIO_PORT, &GPIO_InitStruct); USART_InitStruct.USART_BaudRate = 57600; // the baudrate is set to the value we passed into this init function USART_InitStruct.USART_WordLength = USART_WordLength_8b;// we want the data frame size to be 8 bits (standard) USART_InitStruct.USART_StopBits = USART_StopBits_1; // we want 1 stop bit (standard) USART_InitStruct.USART_Parity = USART_Parity_No; // we don't want a parity bit (standard) USART_InitStruct.USART_HardwareFlowControl = USART_HardwareFlowControl_None; // we don't want flow control (standard) USART_InitStruct.USART_Mode = USART_Mode_Tx | USART_Mode_Rx; // we want to enable the transmitter and the receiver USART_Init(UART_USER, &USART_InitStruct); USART_ITConfig(UART_USER, USART_IT_RXNE, ENABLE); // enable the usart receive interrupt NVIC_InitStructure.NVIC_IRQChannel = USART2_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; // this sets the priority group of the USART1 interrupts NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; // this sets the subpriority inside the group NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; // the USART interrupts are globally enabled NVIC_Init(&NVIC_InitStructure); // the properties are passed to the NVIC_Init function which takes care of the low level stuff USART_Cmd(UART_USER, ENABLE); } I think all the init function is good, what do you think ? My HSE_VALUE is 12MHz, so BRR should be equal to 209. I've 200. It is a problem ? I send 'a', 'b', 'c' ... 'j' and i receive '..j.+....j.+..'2014-07-30 9:40 AM
It's suggestive that it thinks the APB clock is 11520000 Hz
RCC_ClocksTypeDef RCC_ClocksStatus;
RCC_GetClocksFreq(&RCC_ClocksStatus);
printf(''%d %d
'',RCC_ClocksStatus.PCLK1_Frequency, RCC_ClocksStatus.PCLK2_Frequency);
Can you ZIP up a small and complete project (for Keil, IAR or GNU/GCC), including the system_stm32f10x.c file and any PLL settings.
2014-07-30 11:53 PM
I will zip my project, but you talk about PLL settings, are they not call in the system_stm32f1x.c file ?
________________ Attachments : workspace.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0Z8&d=%2Fa%2F0X0000000baS%2FWbEHFpv1V.r2.7m1c_MVMNEegdHhDUs0WucwCF_iivE&asPdf=false2014-07-31 12:10 AM
In system_stm32f10x.c, the function configure PLL1 and PLL2 but enable just PLL2. Shall I enable PLL aswell ?
#ifdef STM32F10X_CL
/* Configure PLLs ------------------------------------------------------*/
/* PLL configuration: PLLCLK = PREDIV1 * 9 = 36 MHz */
RCC->CFGR &= (uint32_t)~(RCC_CFGR_PLLXTPRE | RCC_CFGR_PLLSRC | RCC_CFGR_PLLMULL);
RCC->CFGR |= (uint32_t)(RCC_CFGR_PLLXTPRE_PREDIV1 | RCC_CFGR_PLLSRC_PREDIV1 |
RCC_CFGR_PLLMULL9);
/*!< PLL2 configuration: PLL2CLK = (HSE / 5) * 8 = 40 MHz */
/* PREDIV1 configuration: PREDIV1CLK = PLL2 / 10 = 4 MHz */
RCC->CFGR2 &= (uint32_t)~(RCC_CFGR2_PREDIV2 | RCC_CFGR2_PLL2MUL |
RCC_CFGR2_PREDIV1 | RCC_CFGR2_PREDIV1SRC);
RCC->CFGR2 |= (uint32_t)(RCC_CFGR2_PREDIV2_DIV5 | RCC_CFGR2_PLL2MUL8 |
RCC_CFGR2_PREDIV1SRC_PLL2 | RCC_CFGR2_PREDIV1_DIV10);
/* Enable PLL2 */
RCC->CR |= RCC_CR_PLL2ON;
/* Wait till PLL2 is ready */
while
((RCC->CR & RCC_CR_PLL2RDY) == 0)
{
}
2014-07-31 12:38 AM
RCC_ClocksTypeDef RCC_ClocksStatus;
RCC_GetClocksFreq(&RCC_ClocksStatus); When I look at RCC_ClocksStatus, I have :
SYSCLK = 23MHz
HCLK = 23MHz
PCLK1 = 11520000
PCLK2 = 23Mhz
ADCCLK = 11520000
2014-07-31 8:37 AM
Most of your object files suggest HSE_VALUE is 8000000
printf(''%d '', HSE_VALUE); You should probably adjust your PLL setting, so as not to assume a 25 MHz crystal#ifdef STM32F10X_CL
/* Configure PLLs ------------------------------------------------------*/
/* PLL configuration: PLLCLK = PREDIV1 * 9 = 36 MHz - where PREDIV1 is 4 MHz, see below */
RCC->CFGR &= (uint32_t)~(RCC_CFGR_PLLXTPRE | RCC_CFGR_PLLSRC | RCC_CFGR_PLLMULL);
RCC->CFGR |= (uint32_t)(RCC_CFGR_PLLXTPRE_PREDIV1 | RCC_CFGR_PLLSRC_PREDIV1 |
RCC_CFGR_PLLMULL9);
/*!<
PLL2
configuration: PLL2CLK = (HSE / 3) *
10
=
40
MHz - where HSE is 12 MHz */
/* PREDIV1 configuration:
PREDIV1CLK
=
PLL2
/
10
=
4
MHz */
RCC->CFGR2 &= (uint32_t)~(RCC_CFGR2_PREDIV2 | RCC_CFGR2_PLL2MUL |
RCC_CFGR2_PREDIV1 | RCC_CFGR2_PREDIV1SRC);
RCC->CFGR2 |= (uint32_t)(RCC_CFGR2_PREDIV2_DIV3 | RCC_CFGR2_PLL2MUL10 |
RCC_CFGR2_PREDIV1SRC_PLL2 | RCC_CFGR2_PREDIV1_DIV10);
/* Enable PLL2 */
RCC->CR |= RCC_CR_PLL2ON;
/* Wait till PLL2 is ready */
while((RCC->CR & RCC_CR_PLL2RDY) == 0)
{
}
2014-07-31 8:46 AM
The actual speed you're running at is
((((12 / 5) * 8) / 10) * 9) = 17.28 MHz The machine thinks you're running at ((((8 / 5) * 8) / 10) * 9) = 11.52 MHz The discrepancy here means your baud clock is wrong. You could measure the 17.28 MHz at the MCO pin if you tried.2014-07-31 8:49 AM
((((12 / 3) * 10) / 10) * 9) = 36.00 MHz