2025-11-19 1:55 AM - last edited on 2025-11-19 1:57 AM by mƎALLEm
Hi everyone!
I'm trying to figure out what's wrong with my SPI Peripheral continous transmitting/receiving via DMA in Circular Mode. I think I have coded a pretty basic "Hello, World" for working with DMA, I've just generated code from .ioc file and then added a simple logic. This is my main.c:
/* USER CODE BEGIN Header */
/**
******************************************************************************
* @file : main.c
* @brief : Main program body
******************************************************************************
* @attention
*
* Copyright (c) 2025 STMicroelectronics.
* All rights reserved.
*
* This software is licensed under terms that can be found in the LICENSE file
* in the root directory of this software component.
* If no LICENSE file comes with this software, it is provided AS-IS.
*
******************************************************************************
*/
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
#include "dma.h"
#include "spi.h"
#include "usart.h"
#include "usb_otg.h"
#include "gpio.h"
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
/* USER CODE END Includes */
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
/* USER CODE END PTD */
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
#define SPI3_BUFFER_SIZE 2
/* USER CODE END PD */
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
/* USER CODE END PM */
/* Private variables ---------------------------------------------------------*/
/* USER CODE BEGIN PV */
volatile uint8_t spi3_tx_buffer[SPI3_BUFFER_SIZE] = {0};
volatile uint8_t spi3_rx_buffer[SPI3_BUFFER_SIZE] = {0};
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
/* USER CODE BEGIN PFP */
void SPI3_Start_Comm(void);
/* USER CODE END PFP */
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
/* USER CODE END 0 */
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_DMA_Init();
MX_USART3_UART_Init();
MX_USB_OTG_FS_PCD_Init();
MX_SPI3_Init();
/* USER CODE BEGIN 2 */
SPI3_Start_Comm();
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
/**
* @brief System Clock Configuration
* @retval None
*/
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Configure LSE Drive Capability
*/
HAL_PWR_EnableBkUpAccess();
/** Configure the main internal regulator output voltage
*/
__HAL_RCC_PWR_CLK_ENABLE();
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_BYPASS;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL.PLLM = 4;
RCC_OscInitStruct.PLL.PLLN = 216;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
RCC_OscInitStruct.PLL.PLLQ = 9;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Activate the Over-Drive mode
*/
if (HAL_PWREx_EnableOverDrive() != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_7) != HAL_OK)
{
Error_Handler();
}
}
/* USER CODE BEGIN 4 */
/**
* @brief This function starts SPI Communication for Peripheral device
* @retval None
*/
void SPI3_Start_Comm(void)
{
HAL_SPI_TransmitReceive_DMA(&hspi3,(uint8_t*)spi3_tx_buffer,
(uint8_t*)spi3_rx_buffer,SPI3_BUFFER_SIZE);
}
void HAL_SPI_TxRxCpltCallback(SPI_HandleTypeDef *hspi)
{
if(hspi->Instance == SPI3)
{
spi3_tx_buffer[0] = spi3_rx_buffer[0];
spi3_tx_buffer[1] = spi3_rx_buffer[1];
}
}
/* USER CODE END 4 */
/**
* @brief This function is executed in case of error occurrence.
* @retval None
*/
void Error_Handler(void)
{
/* USER CODE BEGIN Error_Handler_Debug */
/* User can add his own implementation to report the HAL error return state */
__disable_irq();
while (1)
{
}
/* USER CODE END Error_Handler_Debug */
}
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* file: pointer to the source file name
* line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t *file, uint32_t line)
{
/* USER CODE BEGIN 6 */
/* User can add his own implementation to report the file name and line number,
ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
/* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */
As you can see, I just start communication in SPI3_Start_Comm() and then in HAL_SPI_TxRxCpltCallback I prepare the bytes received at N-time to echo back at N+1-time.
What I get is the peripheral echoing back bytes at N+x-time, after three or four garbage results at first. If I print results from controller point of view this is what I get:
COPI CIPO
0: 0000 XXXX (garbage)
1: 0000 XXXX (garbage)
2: 0800 XXXX (garbage)
3: 0800 XXXX (garbage)
4: 1000 0000 (N+3 echo back - it should be N+1 or 0800). Missing N = 0 echo
5: 1000 0800 (and so on...)
6: 1800 0800
7: 1800 1000
8: 2000 1000
9: 2000 1800
10: 2800 1800
11: 2800 2000
12: 3000 2000
13: 3000 2800
14: 3800 2800
15: 3800 3000
16: 0000 3000
17: 0000 3800
18: 0800 3800
19: 0800 0000
20: 1000 0000
...
Peripheral device is STM32F722ZE. Controller is a black box.
Here's my spi.c and dma.c files generated from .ioc:
spi.c:
/* USER CODE BEGIN Header */
/**
******************************************************************************
* @file spi.c
* @brief This file provides code for the configuration
* of the SPI instances.
******************************************************************************
* @attention
*
* Copyright (c) 2025 STMicroelectronics.
* All rights reserved.
*
* This software is licensed under terms that can be found in the LICENSE file
* in the root directory of this software component.
* If no LICENSE file comes with this software, it is provided AS-IS.
*
******************************************************************************
*/
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "spi.h"
/* USER CODE BEGIN 0 */
/* USER CODE END 0 */
SPI_HandleTypeDef hspi3;
DMA_HandleTypeDef hdma_spi3_rx;
DMA_HandleTypeDef hdma_spi3_tx;
/* SPI3 init function */
void MX_SPI3_Init(void)
{
/* USER CODE BEGIN SPI3_Init 0 */
/* USER CODE END SPI3_Init 0 */
/* USER CODE BEGIN SPI3_Init 1 */
/* USER CODE END SPI3_Init 1 */
hspi3.Instance = SPI3;
hspi3.Init.Mode = SPI_MODE_SLAVE;
hspi3.Init.Direction = SPI_DIRECTION_2LINES;
hspi3.Init.DataSize = SPI_DATASIZE_8BIT;
hspi3.Init.CLKPolarity = SPI_POLARITY_HIGH;
hspi3.Init.CLKPhase = SPI_PHASE_2EDGE;
hspi3.Init.NSS = SPI_NSS_HARD_INPUT;
hspi3.Init.FirstBit = SPI_FIRSTBIT_MSB;
hspi3.Init.TIMode = SPI_TIMODE_DISABLE;
hspi3.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
hspi3.Init.CRCPolynomial = 7;
hspi3.Init.CRCLength = SPI_CRC_LENGTH_DATASIZE;
hspi3.Init.NSSPMode = SPI_NSS_PULSE_DISABLE;
if (HAL_SPI_Init(&hspi3) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN SPI3_Init 2 */
/* USER CODE END SPI3_Init 2 */
}
void HAL_SPI_MspInit(SPI_HandleTypeDef* spiHandle)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
if(spiHandle->Instance==SPI3)
{
/* USER CODE BEGIN SPI3_MspInit 0 */
/* USER CODE END SPI3_MspInit 0 */
/* SPI3 clock enable */
__HAL_RCC_SPI3_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
__HAL_RCC_GPIOB_CLK_ENABLE();
/**SPI3 GPIO Configuration
PA4 ------> SPI3_NSS
PB3 ------> SPI3_SCK
PB4 ------> SPI3_MISO
PB5 ------> SPI3_MOSI
*/
GPIO_InitStruct.Pin = GPIO_PIN_4;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF6_SPI3;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_3|GPIO_PIN_4|GPIO_PIN_5;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF6_SPI3;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
/* SPI3 DMA Init */
/* SPI3_RX Init */
hdma_spi3_rx.Instance = DMA1_Stream0;
hdma_spi3_rx.Init.Channel = DMA_CHANNEL_0;
hdma_spi3_rx.Init.Direction = DMA_PERIPH_TO_MEMORY;
hdma_spi3_rx.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_spi3_rx.Init.MemInc = DMA_MINC_ENABLE;
hdma_spi3_rx.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;
hdma_spi3_rx.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;
hdma_spi3_rx.Init.Mode = DMA_CIRCULAR;
hdma_spi3_rx.Init.Priority = DMA_PRIORITY_VERY_HIGH;
hdma_spi3_rx.Init.FIFOMode = DMA_FIFOMODE_DISABLE;
if (HAL_DMA_Init(&hdma_spi3_rx) != HAL_OK)
{
Error_Handler();
}
__HAL_LINKDMA(spiHandle,hdmarx,hdma_spi3_rx);
/* SPI3_TX Init */
hdma_spi3_tx.Instance = DMA1_Stream5;
hdma_spi3_tx.Init.Channel = DMA_CHANNEL_0;
hdma_spi3_tx.Init.Direction = DMA_MEMORY_TO_PERIPH;
hdma_spi3_tx.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_spi3_tx.Init.MemInc = DMA_MINC_ENABLE;
hdma_spi3_tx.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;
hdma_spi3_tx.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;
hdma_spi3_tx.Init.Mode = DMA_CIRCULAR;
hdma_spi3_tx.Init.Priority = DMA_PRIORITY_VERY_HIGH;
hdma_spi3_tx.Init.FIFOMode = DMA_FIFOMODE_DISABLE;
if (HAL_DMA_Init(&hdma_spi3_tx) != HAL_OK)
{
Error_Handler();
}
__HAL_LINKDMA(spiHandle,hdmatx,hdma_spi3_tx);
/* SPI3 interrupt Init */
HAL_NVIC_SetPriority(SPI3_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(SPI3_IRQn);
/* USER CODE BEGIN SPI3_MspInit 1 */
/* USER CODE END SPI3_MspInit 1 */
}
}
void HAL_SPI_MspDeInit(SPI_HandleTypeDef* spiHandle)
{
if(spiHandle->Instance==SPI3)
{
/* USER CODE BEGIN SPI3_MspDeInit 0 */
/* USER CODE END SPI3_MspDeInit 0 */
/* Peripheral clock disable */
__HAL_RCC_SPI3_CLK_DISABLE();
/**SPI3 GPIO Configuration
PA4 ------> SPI3_NSS
PB3 ------> SPI3_SCK
PB4 ------> SPI3_MISO
PB5 ------> SPI3_MOSI
*/
HAL_GPIO_DeInit(GPIOA, GPIO_PIN_4);
HAL_GPIO_DeInit(GPIOB, GPIO_PIN_3|GPIO_PIN_4|GPIO_PIN_5);
/* SPI3 DMA DeInit */
HAL_DMA_DeInit(spiHandle->hdmarx);
HAL_DMA_DeInit(spiHandle->hdmatx);
/* SPI3 interrupt Deinit */
HAL_NVIC_DisableIRQ(SPI3_IRQn);
/* USER CODE BEGIN SPI3_MspDeInit 1 */
/* USER CODE END SPI3_MspDeInit 1 */
}
}
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
dma.c:
/* USER CODE BEGIN Header */
/**
******************************************************************************
* @file dma.c
* @brief This file provides code for the configuration
* of all the requested memory to memory DMA transfers.
******************************************************************************
* @attention
*
* Copyright (c) 2025 STMicroelectronics.
* All rights reserved.
*
* This software is licensed under terms that can be found in the LICENSE file
* in the root directory of this software component.
* If no LICENSE file comes with this software, it is provided AS-IS.
*
******************************************************************************
*/
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "dma.h"
/* USER CODE BEGIN 0 */
/* USER CODE END 0 */
/*----------------------------------------------------------------------------*/
/* Configure DMA */
/*----------------------------------------------------------------------------*/
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/**
* Enable DMA controller clock
*/
void MX_DMA_Init(void)
{
/* DMA controller clock enable */
__HAL_RCC_DMA1_CLK_ENABLE();
/* DMA interrupt init */
/* DMA1_Stream0_IRQn interrupt configuration */
HAL_NVIC_SetPriority(DMA1_Stream0_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(DMA1_Stream0_IRQn);
/* DMA1_Stream1_IRQn interrupt configuration */
HAL_NVIC_SetPriority(DMA1_Stream1_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(DMA1_Stream1_IRQn);
/* DMA1_Stream3_IRQn interrupt configuration */
HAL_NVIC_SetPriority(DMA1_Stream3_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(DMA1_Stream3_IRQn);
/* DMA1_Stream5_IRQn interrupt configuration */
HAL_NVIC_SetPriority(DMA1_Stream5_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(DMA1_Stream5_IRQn);
}
/* USER CODE BEGIN 2 */
/* USER CODE END 2 */
What am I missing?
Thanks to anyone who will try to help!
2025-11-19 2:14 AM
In the code above, you start SPI transfer only once and you don't print anything.
Show the code in which you experience the problem - with transfer restart and result printing.
2025-11-19 2:27 AM
As @gbm said above, debug from the STM32 perspective, as you appear not to know how exactly does the master behave. A good way to start would be to observe the SPI waveforms using oscilloscope/logic analyz
Note, that SPI has a FIFO. How is SPIx_CR2.FRXTH set?
JW
2025-11-19 3:02 AM
thanks @waclawek.jan and @gbm, since controller is a black box I can only debug the STM32 (even if I can see print from master, as I posted).
HAL_SPI_TxRxCpltCallback is properly triggered each time the peripheral receives a request from the controller, so I am assuming that it is something about DMA circular buffer pointer (buffer collect indeed the received bytes, but the DMA sends those bytes back after two more transactions). Does it sound reasonable to you?
Also, does my code look correct to you?
Thanks,
GT
2025-11-19 3:31 AM - edited 2025-11-19 3:32 AM
> Note, that SPI has a FIFO. How is SPIx_CR2.FRXTH set?
Yes, a problem I came across while porting some example code for SPI using DMA.
The RM explicitely states :
Configure the FRXTH bit. The RXFIFO threshold must be aligned to the read access size for the SPIx_DR register.
2025-11-19 3:45 AM
> DMA sends those bytes back after two more transactions
Now it dawned on me.
SPI has a 4-byte (32-bit) Tx FIFO. As soon as you enable SPI (and DMA in it), it sets TXE and that remains to be sent until FIFO is filled. DMA, when it sees TXE set, transfers data into SPI, so as soon as SPI/DMA is enabled, the FIFO is immediately filled up. That's your "garbage" at the beginning, the 4 extra bytes you see.
If I am not mistaken, there's no workaround.
JW
2025-11-19 5:00 AM
> If I am not mistaken, there's no workaround.
Perhaps by pre-filling the FIFO manually, and subtracting the 4 bytes from the DMA transfer.
But I rarely dealt with DMA in connection to SPI, most of my use cases were short transfer sequences based upon previous transfers, and thus interrupt-driven.
2025-11-19 7:57 AM
> Perhaps by pre-filling the FIFO manually, and subtracting the 4 bytes from the DMA transfer.
That won't help with the lag - those 4 bytes would get "into the queue", regardless of whether it's through DMA or manually.
What would work is to transfer bytes to Tx not based on TXE, but as they arrive - using a single DMA triggered by RXNE and transferring from SPI_DR to SPI_DR - but this would be just an exercise anyway with no practical application, as the data then could not be stored in RAM and processed further.
JW
2025-11-19 8:20 AM
I'm trying different things here, but I wasn't able to edit SPI registers (maybe I should set some bit somewhere to enable SPI register write?).
Anyway, out of hope I tried to edit SPI data size and observed the behavior change significantly. Now, setting data size = 4 bits, I don't have shifted transaction anymore, but MSB and LSB seems to be inverted:
/* SPI3 init function */
void MX_SPI3_Init(void)
{
/* USER CODE BEGIN SPI3_Init 0 */
/* USER CODE END SPI3_Init 0 */
/* USER CODE BEGIN SPI3_Init 1 */
/* USER CODE END SPI3_Init 1 */
hspi3.Instance = SPI3;
hspi3.Init.Mode = SPI_MODE_SLAVE;
hspi3.Init.Direction = SPI_DIRECTION_2LINES;
hspi3.Init.DataSize = SPI_DATASIZE_4BIT;
hspi3.Init.CLKPolarity = SPI_POLARITY_HIGH;
hspi3.Init.CLKPhase = SPI_PHASE_2EDGE;
hspi3.Init.NSS = SPI_NSS_HARD_INPUT;
hspi3.Init.FirstBit = SPI_FIRSTBIT_MSB;
hspi3.Init.TIMode = SPI_TIMODE_DISABLE;
hspi3.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
hspi3.Init.CRCPolynomial = 7;
hspi3.Init.CRCLength = SPI_CRC_LENGTH_DATASIZE;
hspi3.Init.NSSPMode = SPI_NSS_PULSE_DISABLE;
if (HAL_SPI_Init(&hspi3) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN SPI3_Init 2 */
/* USER CODE END SPI3_Init 2 */
}Output now is:
COPI CIPO
0: 0000 0038
1: 0000 0000
2: 0800 0000
3: 0800 0008
4: 1000 0008
5: 1000 0010
6: 1800 0010
7: 1800 0018
8: 2000 0018
9: 2000 0020
I really don't understand and yes, I even tried to set first bit LSB and nothing change (even stranger).
Any clues?
2025-11-20 12:47 AM
> I don't have shifted transaction anymore
You still do, and the reason is still the Tx FIFO, except this time the "garbage" is four 4-bit nibble (which in STM32 is stored/transferred as 4 bytes with only LSB containing the bits coming from/going to SPI), showing up in your printout as two bytes; the third byte (which is two 4-bit nibble) is the "natural" delay given by the 2-byte Rx-DMA-to-Tx-DMA transfer (i.e. the size of buffers in memory and the DMA transfer size).
What you should do is:
- replace the master with a master written by you, over which you have full control; it may even be (and it would even be better) a bit-banged one on the same STM32
- after each frame, observe e.g. in debugger, what is the state of the DMA (mainly NDTR) and SPI (mainly the FIFO status bits) registers, and what is in the buffers in memory
- draw yourself a diagram with the individual items in the chain (i.e. SPI receiver, SPI Rx FIFO, DMA/Rx memory buffer, DMA/Tx memory buffer, SPI Tx FIFO, SPI transmitter), and after each step, write down what data do you have in which item according to your understanding, and then compare with reality
JW