2019-04-10 8:43 AM
STM32 v 1.10, DBGMCU FREEZE / UNFREEZE Macros have been renamed and are located in stm32f3xx_hal.h
WHY do they have inconsistent names? Snippet of definitions below from lines 500-530 of stm32f3xx_hal.h
#if defined(DBGMCU_APB1_FZ_DBG_WWDG_STOP)
#define __HAL_DBGMCU_FREEZE_WWDG() (DBGMCU->APB1FZ |= (DBGMCU_APB1_FZ_DBG_WWDG_STOP))
#define __HAL_DBGMCU_UNFREEZE_WWDG() (DBGMCU->APB1FZ &= ~(DBGMCU_APB1_FZ_DBG_WWDG_STOP))
#endif /* DBGMCU_APB1_FZ_DBG_WWDG_STOP */
#if defined(DBGMCU_APB1_FZ_DBG_IWDG_STOP)
#define __HAL_DBGMCU_FREEZE_IWDG() (DBGMCU->APB1FZ |= (DBGMCU_APB1_FZ_DBG_IWDG_STOP))
#define __HAL_DBGMCU_UNFREEZE_IWDG() (DBGMCU->APB1FZ &= ~(DBGMCU_APB1_FZ_DBG_IWDG_STOP))
#endif /* DBGMCU_APB1_FZ_DBG_IWDG_STOP */
#if defined(DBGMCU_APB1_FZ_DBG_I2C1_SMBUS_TIMEOUT)
#define __HAL_DBGMCU_FREEZE_I2C1_TIMEOUT() (DBGMCU->APB1FZ |= (DBGMCU_APB1_FZ_DBG_I2C1_SMBUS_TIMEOUT))
#define __HAL_DBGMCU_UNFREEZE_I2C1_TIMEOUT() (DBGMCU->APB1FZ &= ~(DBGMCU_APB1_FZ_DBG_I2C1_SMBUS_TIMEOUT))
#endif /* DBGMCU_APB1_FZ_DBG_I2C1_SMBUS_TIMEOUT */
#if defined(DBGMCU_APB1_FZ_DBG_I2C2_SMBUS_TIMEOUT)
#define __HAL_DBGMCU_FREEZE_I2C2_TIMEOUT() (DBGMCU->APB1FZ |= (DBGMCU_APB1_FZ_DBG_I2C2_SMBUS_TIMEOUT))
#define __HAL_DBGMCU_UNFREEZE_I2C2_TIMEOUT() (DBGMCU->APB1FZ &= ~(DBGMCU_APB1_FZ_DBG_I2C2_SMBUS_TIMEOUT))
#endif /* DBGMCU_APB1_FZ_DBG_I2C2_SMBUS_TIMEOUT */
#if defined(DBGMCU_APB1_FZ_DBG_I2C3_SMBUS_TIMEOUT)
#define __HAL_DBGMCU_FREEZE_I2C3_TIMEOUT() (DBGMCU->APB1FZ |= (DBGMCU_APB1_FZ_DBG_I2C3_SMBUS_TIMEOUT))
#define __HAL_DBGMCU_UNFREEZE_I2C3_TIMEOUT() (DBGMCU->APB1FZ &= ~(DBGMCU_APB1_FZ_DBG_I2C3_SMBUS_TIMEOUT))
#endif /* DBGMCU_APB1_FZ_DBG_I2C3_SMBUS_TIMEOUT */
#if defined(DBGMCU_APB1_FZ_DBG_CAN_STOP)
#define __HAL_FREEZE_CAN_DBGMCU() (DBGMCU->APB1FZ |= (DBGMCU_APB1_FZ_DBG_CAN_STOP))
#define __HAL_UNFREEZE_CAN_DBGMCU() (DBGMCU->APB1FZ &= ~(DBGMCU_APB1_FZ_DBG_CAN_STOP))
#endif /* DBGMCU_APB1_FZ_DBG_CAN_STOP */
/**Most macros are __HAL_DBGMCU_FREEZE_PERIPH and __HAL_DBGMCU_UNFREEZE_PERIPH, but a small percentage of them are __HAL_FREEZE_PERIPH_DBGMCU and __HAL_UNFREEZE_PERIPH_DBGMCU.
I suppose this is more of a gripe / notification post, but I'd be curios if there is a reason for the inconsistency.