cancel
Showing results for 
Search instead for 
Did you mean: 

Which class of USB is used for making the communication between the STM and Application ?

MDeva.1
Associate II

Helllo,

I am working on Nucleo-h745ziq board. Using the GUI I creating the application of 3 LED and one user button. When I press the switch the led starts the blinking on stm32,For this purpose which Usb class that I have use HID or Custome HId. Can you please help me. If there is example like that in cubemx can you suggest me.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0