cancel
Showing results for 
Search instead for 
Did you mean: 

When the USB is de-initialized with USBD_DeInit(..) the USB tranceiver is not put in powerdown.

Bvan .13
Associate

Our product uses the embedded USB PHY and only initialize the USB CDC when needed. Any other time we keep it de-initialized. At initialization the tranceiver is enabled through HAL_PCD_Init() that uses the function USB_CoreInit(). When de-initialized with HAL_PCD_DeInit() the tranceiver is not placed in powerdown (PWRDWN bit in register OTG_GCCFG).

The PWRDWN bit should be reset in the method HAL_PCD_DevConnect().

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0