2020-10-18 7:10 AM
I am using a custom bootloader in STM32F091RB controller (cortex M0) which has a system clock of 8MHz and my application STM32F091VC controller (cortex M0) has system clock of 48MHz. Will it affect my application peripheral's interrupt. As my interrupts are not working. I have also mapped vector table to SRAM and again remapped it to 0x00000000. Though its not working.
Below is from bootloader code.
#define SRAM_BASE_ADDR 0x20000000
#define CODE_SLOT_1_BASE_ADDR (uint32_t)0x08002100
#define CODE_SLOT_2_BASE_ADDR (uint32_t)0x08019000
void fnJumpToApp(void)
{
uint8_t i;
uint32_t *p = (uint32_t *)SRAM_BASE_ADDR; // Base of RAM (0xC0 carved out in scatter file)
uint32_t *q = (uint32_t *)CODE_SLOT_1_BASE_ADDR; // Base of FLASH
__disable_irq();
/* Relocate by software the vector table to the internal SRAM at 0x20000000 ***/
/* Copy the vector table from the Flash (mapped at the base of the application
load address 0x08000000) to the base address of the SRAM at 0x20000000. */
for(i=0; i<48; i++)
*p++ = *q++;
/* Enable the SYSCFG peripheral clock*/
RCC_APB2PeriphResetCmd(RCC_APB2Periph_SYSCFG, ENABLE);
/* Remap SRAM at 0x00000000 */
SYSCFG_MemoryRemapConfig(SYSCFG_MemoryRemap_SRAM);
/* Set system control register SCR->VTOR */
uliJumpAddress = *(uint32_t*) (CODE_SLOT_1_BASE_ADDR + 4);
Jump_To_Application = (pFunction) uliJumpAddress;
__set_MSP(*(uint32_t*) CODE_SLOT_1_BASE_ADDR);
Jump_To_Application();
}Below is from the application code.
void fnRemapVectorTable(void)
{
uint8_t i;
uint32_t *p = (uint32_t *)SRAM_BASE_ADDR; // Base of RAM (0xC0 carved out in scatter file)
uint32_t *q = (uint32_t *)CODE_SLOT_1_BASE_ADDR; // Base of FLASH
/* Relocate by software the vector table to the internal SRAM at 0x20000000 ***/
/* Copy the vector table from the Flash (mapped at the base of the application
load address 0x08000000) to the base address of the SRAM at 0x20000000. */
for(i=0; i<48; i++)
*p++ = *q++;
/* Enable the SYSCFG peripheral clock*/
RCC_APB2PeriphResetCmd(RCC_APB2Periph_SYSCFG, ENABLE);
RCC_APB2PeriphClockCmd (RCC_APB2Periph_SYSCFG, ENABLE);
/* Remap SRAM at 0x00000000 */
SYSCFG_MemoryRemapConfig(SYSCFG_MemoryRemap_SRAM);
__enable_irq();
}
can anyone please help me out?
Solved! Go to Solution.
2020-10-18 9:31 AM
I mean your idea have some mistakes. As first why relocate in bootloader ? We use only jump to app and relocate in start app sequence.
example from 03X but i mean no dif with 09x
__IO uint32_t VectorTable[48] __attribute__((at(0x20000000)));
void IAP_Config(void)
{
uint8_t i = 0;
// Relocate by software the vector table to the internal SRAM at 0x20000000
// Copy the vector table from the Flash (mapped at the base of the application
// load address 0x0800x000) to the base address of the SRAM at 0x20000000
for(i = 0; i < 48; i++) VectorTable[i] = *(__IO uint32_t*)(APPLICATION_ADDRESS + (i<<2));
// Remap SRAM at 0x00000000
SYSCFG_MemoryRemapConfig(SYSCFG_MemoryRemap_SRAM);
}
too i dont uderstand why you copy vectors from ap1 but jump to ap2
and maybe your compiler make mis when try *p++ = *q++;
Plus when you relocate to ram you need reserve this ram in map.
2020-10-18 7:36 AM
> I am using a custom bootloader in STM32F091RB controller (cortex M0) which has a system clock of 8MHz and my application STM32F091VC controller (cortex M0) has system clock of 48MHz.
You have a bootloader on a separate chip from your application? I would attach a debugger to the chip you're trying to debug and see what "not working" actually means. Ensure you're not in an interrupt context. Ensure interrupts are enabled.
2020-10-18 8:06 AM
Lose the RCC_APB2PeriphResetCmd(RCC_APB2Periph_SYSCFG, ENABLE); in both cases. Use RCC_APB2PeriphClockCmd(RCC_APB2Periph_SYSCFG, ENABLE);
To reset the unit you must enable then disable the internal reset node
2020-10-18 9:31 AM
I mean your idea have some mistakes. As first why relocate in bootloader ? We use only jump to app and relocate in start app sequence.
example from 03X but i mean no dif with 09x
__IO uint32_t VectorTable[48] __attribute__((at(0x20000000)));
void IAP_Config(void)
{
uint8_t i = 0;
// Relocate by software the vector table to the internal SRAM at 0x20000000
// Copy the vector table from the Flash (mapped at the base of the application
// load address 0x0800x000) to the base address of the SRAM at 0x20000000
for(i = 0; i < 48; i++) VectorTable[i] = *(__IO uint32_t*)(APPLICATION_ADDRESS + (i<<2));
// Remap SRAM at 0x00000000
SYSCFG_MemoryRemapConfig(SYSCFG_MemoryRemap_SRAM);
}
too i dont uderstand why you copy vectors from ap1 but jump to ap2
and maybe your compiler make mis when try *p++ = *q++;
Plus when you relocate to ram you need reserve this ram in map.
2020-10-18 12:22 PM
No. Actually my controller is STM32F091RB but ky bootloader project has device as STM32F091RB but my application project has device as STM32F091VC. Will it cause to interrupt issue?
2020-10-19 12:05 AM
How IDE you use ? Keil , IAR, CubeIDE? I mean you dont setup RAM shift and app use RAM from address zero, then any variables overwrite your interrupt vector table values.