cancel
Showing results for 
Search instead for 
Did you mean: 

USB transferring data in a composite device (DUAL CDC)

moulay-hassan
Associate II
Posted on May 30, 2016 at 08:30

I have emulated two VCPs with only one USB Device. I can send data in one VCP that has the following Endpoint Address.

#define CDC_IN_EP 0x81 /* EP1 for data IN */#define CDC_OUT_EP 0x01 /* EP1 for data OUT */#define CDC_CMD_EP 0x82 /* EP2 for CDC commands */

I would like to know if it's possible to send data in the other VCP with other Endpoint Address like :

#define CDC_IN_EP3 0x83 /* EP3 for data IN */#define CDC_OUT_EP3 0x03 /* EP3 for data OUT */#define CDC_CMD_EP4 0x84 /* EP4 for CDC commands */

My problem is that addresses others than 0x81 don't allow me to send data over the second VCP. I'm using two CDC interfaces Full-Speed. Normally we can use 7 endpoints with CDC_FS and that's what I'm trying to do.. I have 6 Endpoints: 3 for each VCP and the seventh is Endpoint 0 for configuration.

Have I missed something in the Endpoints Configuration or in the Composite Device Descriptors ?

Thank you guys.

#usb #stm32 #usb #cdc #cdc #vcp #endpoints
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Walid FTITI_O
Senior II
moulay-hassan
Associate II
Posted on May 31, 2016 at 08:48

The original post was too long to process during our migration. Please click on the provided URL to read the original post. https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I6Wh&d=%2Fa%2F0X0000000bpy%2FslcbqW7OdA9Dm3bdhbXBZhQldPvLSQELwrrFyQrx1YY&asPdf=false