Skip to main content
fb2
Associate II
August 31, 2015
Question

USB Printer Class: Cannot print

  • August 31, 2015
  • 0 replies
  • 556 views
Posted on August 31, 2015 at 15:31

Hello to all,

I'm trying to implement a printer class for the USB. Currently I'm using the STM32F4 Discovery.

I already have working the detection of the printer (EPSON CX5600) , reading the ID, etc.

What I cant make work is printing. I'm sending via bulk out ESCPOS commands, but nothing goes out of the printer. The only thing that happens is that, if the printer goes to sleep because of long time of inactivity, when I send the commands to print, the print awakes.

Does anybody have more information or any experience on this?

Thanks to all.

Regards

Fernando

#usb #printer #epson
This topic has been closed for replies.