Skip to main content
harry anders
Associate III
July 31, 2021
Question

USB Mass Storage and SDCARD on STM32F7 not working.

  • July 31, 2021
  • 1 reply
  • 803 views

I have a hardware with STM32F777BIT6 MCU. Base for original code was generated using an older version of STMCUBE about 3 years ago. SDcard works fine with FAT file system and I can read and write to it without a problem. USB also works fine and I am using it in virtual serial port mode with out a problem.

Recently, we need to use the device as USB Mass storage device. I have tried looking for some examples but they are not compatible with my MCU (only work on STM32F1 or STM32F4). I tried to merge those examples with my own code but without luck. All I manage to see when I connect the hardware to a PC is empty drives. I cannot open the drives or copy anything into them.

What is the problem? Is there an example that is compatible with the MCU I am using or a guide to implement this.

This topic has been closed for replies.

1 reply

ST Technical Moderator
August 17, 2021

Hello @harry anders​ ,

In the STM32CubeF7 package, there are already the USB device application based on the Mass Storage Class (MSC) that you may re-use sections available in the examples or get inspired from them:

\STM32Cube_FW_F7_V1.16.1\Projects\STM32756G_EVAL\Applications\USB_Device\MSC_Standalone

\STM32Cube_FW_F7_V1.16.1\Projects\STM32F769I-Discovery\Applications\USB_Device\MSC_Standalone

Hope my answer helped you!

When your question is answered, please close this topic by choosing Select as Best.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks