cancel
Showing results for 
Search instead for 
Did you mean: 

USB HOST MSC: Function f_findfirst() returns FR_DISK_ERR error despite USB Stick has been successfully mounted

BParh.1
Senior III

I am trying to implement simple appication to scan existing files in USB stick in root directory. I just use ST sample as reference and following is the user call back code. The error is line 27

It manage to reach :

Appli_state = APPLICATION_START; and then successful mount f_mount().

Then it hit Appli_state = APPLICATION_READY; and then go here:

fr = f_findfirst(&dj, &fno, "/", "*.txt");

the returned fr so far always give FR_DISK_ERR. But I have verified by USB stick is ok when I use my PC to detect, write and read files.

I'd appreciate if someone can give some pointeres.

I am using STM32F769 Discovery Board and utilizing USB_OTG_HS peripheral as USB Host class MSC.

FRESULT fr;     /* Return value */
DIR dj;         /* Directory object */
FILINFO fno;    /* File information */
 
static void USBH_UserProcess  (USBH_HandleTypeDef *phost, uint8_t id)
{
  /* USER CODE BEGIN CALL_BACK_1 */
  switch(id)
  {
  case HOST_USER_SELECT_CONFIGURATION:
  break;
 
  case HOST_USER_DISCONNECTION:
  Appli_state = APPLICATION_DISCONNECT;
  printf("app disconnect\r\n");
  if(FATFS_UnLinkDriver(USBKey_Path) != 0) {
	  printf("ERROR : Cannot unlink FatFS driver! \n");
  }
  if(f_mount(NULL, "", 0) != FR_OK)
  {
	  printf("ERROR : Cannot DeInitialize FatFs! \n");
  }
  break;
  case HOST_USER_CLASS_ACTIVE:
  Appli_state = APPLICATION_READY;
 
  fr = f_findfirst(&dj, &fno, "/", "*.txt"); // why always returns FR_DISK_ERR ?
   while (fr == FR_OK && fno.fname[0]) {         /* Repeat while an item is found */
  	printf("%s\r\n", fno.fname);                /* Print the object name */
  	fr = f_findnext(&dj, &fno);               /* Search for next item */
   }
  f_closedir(&dj);
  break;
  case HOST_USER_CONNECTION:
  Appli_state = APPLICATION_START;
  printf("app start\r\n");
  if(f_mount(&USBH_FatFs, "", 0) != FR_OK) {
	  printf("ERROR : Cannot Initialize FatFs! \n");
   }
  else {
	  printf("Mount success\r\n");
  }
  break;
 
  default:
  break;
  }
  /* USER CODE END CALL_BACK_1 */
}

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
BParh.1
Senior III

In fact it seems, I cannot do any simple write/read too e.g. f_write() and f_read()