cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H743 STOP mode exit problem with LTDC

sjkarthick
Associate

Entered into low power STOP mode

HAL_PWR_EnterSTOPMode(PWR_LOWPOWERREGULATOR_ON, PWR_STOPENTRY_WFI);

 

Reconfigured LTDC when exiting from STOP mode, LTDC is not driving the display.

SystemClock_Config();
HAL_ResumeTick();
__enable_irq();
MX_LTDC_Init();
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
FBL
ST Employee

Hello @sjkarthick 

 

You need to configure system clock after wake-up from STOP: enable HSE, PLL ... 

You can try this example as a reference using RTC wakeup timer associated to EXTI line flag:

STM32Cube\Repository\STM32Cube_FW_H7_V1.11.1\Projects\STM32H743IEVAL\Examples\PWR\PWR_STOP_RTC 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL