cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F7 NanoEdgeAIstudio

HCYHCZ
Associate

I call the following function:

neai_classification(input_user_buffer, output_class_buffer, &id_class);

When the program runs this function, it enters the following function:

void HardFault_Handler(void)

 

This is the first time to use, if you need other information to help determine the fault location please leave a message, thank you very much

 

The software used is as follows:

STM32CubeIDE 1.14.0

NanoEdgeAIstudio 4.3.0

 

The following hardware is used:

NUCLEO-STM32F746ZGT6

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0