cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F411E-DISCO Audio application Atollic compile woes

FDixo
Associate III

We have a new STM32F411E-DISCO kit and are trying to run the Audio playback and record application.

I have imported the SW4STM32 project but I keep getting errors with missing files - usually the following:

stm32f411e_discovery_accelerometer.c

..\Common\audio.h

stm32f411e_discovery_accelerometer.h

I have found these files and added the paths to the project properties but still cannot compile. Let me know if you can get this to compile. Any help would be much appreciated. Thanks

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Imen.D
ST Employee

Hello @FDixo​ ,

Check your configuration and include paths (check backslash, slash). 

You can share your project to review the defines syntax of include file paths.

With Regards,

Imen.

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
FDixo
Associate III

I am not sure what that means to check the configuration. The paths all have the same slash.

There are some slash issues in the compile below. Also, the local sales rep managed to get the project imported and compiled with no issues whatsoever reportedly. If all else fails we will get them in next week since they are only 2-3 km away.

18:22:26 **** Rebuild of configuration Debug for project STM32F411E-DISCO ****

Info: Internal Builder is used for build

arm-atollic-eabi-gcc -c ..\..\..\..\..\..\..\..\Drivers\STM32F4xx_HAL_Driver\Src\stm32f4xx_hal_i2c.c -mthumb -mcpu=cortex-m4 -mfloat-abi=hard -mfpu=fpv4-sp-d16 -std=gnu11 -DUSE_HAL_DRIVER -DSTM32F411xE -DUSE_STM32F411E_DISCO -I../../../Inc -I../../../../../../../../Drivers/CMSIS/Device/ST/STM32F4xx/Include -I../../../../../../../../Drivers/STM32F4xx_HAL_Driver/Inc -I../../../../../../../../Drivers/BSP/STM32F411E-Discovery -I../../../../../../../../Middlewares/ST/STM32_USB_Device_Library/Core/Inc -I../../../../../../../../Middlewares/ST/STM32_USB_Host_Library/Class/MSC/Inc -I../../../../../../../../Middlewares/ST/STM32_USB_Host_Library/Core/Inc -I../../../../../../../../Middlewares/ST/STM32_Audio/Addons/PDM/Inc -I../../../../../../../../Middlewares/Third_Party/FatFs/src -I../../../../../../../../Drivers/CMSIS/Include -Os -ffunction-sections -g3 -fstack-usage -Wall -fmessage-length=0 -specs=nano.specs -o Drivers\STM32F4xx_HAL_Drivers\stm32f4xx_hal_i2c.o 

arm-atollic-eabi-gcc -c ..\..\..\..\..\..\..\..\Middlewares\Third_Party\FatFs\src\option\unicode.c -mthumb -mcpu=cortex-m4 -mfloat-abi=hard -mfpu=fpv4-sp-d16 -std=gnu11 -DUSE_HAL_DRIVER -DSTM32F411xE -DUSE_STM32F411E_DISCO -I../../../Inc -I../../../../../../../../Drivers/CMSIS/Device/ST/STM32F4xx/Include -I../../../../../../../../Drivers/STM32F4xx_HAL_Driver/Inc -I../../../../../../../../Drivers/BSP/STM32F411E-Discovery -I../../../../../../../../Middlewares/ST/STM32_USB_Device_Library/Core/Inc -I../../../../../../../../Middlewares/ST/STM32_USB_Host_Library/Class/MSC/Inc -I../../../../../../../../Middlewares/ST/STM32_USB_Host_Library/Core/Inc -I../../../../../../../../Middlewares/ST/STM32_Audio/Addons/PDM/Inc -I../../../../../../../../Middlewares/Third_Party/FatFs/src -I../../../../../../../../Drivers/CMSIS/Include -Os -ffunction-sections -g3 -fstack-usage -Wall -fmessage-length=0 -specs=nano.specs -o Middlewares\FatFs\Options\unicode.o 

arm-atollic-eabi-gcc -c ..\..\..\..\..\..\..\..\Middlewares\ST\STM32_USB_Host_Library\Core\Src\usbh_ctlreq.c -mthumb -mcpu=cortex-m4 -mfloat-abi=hard -mfpu=fpv4-sp-d16 -std=gnu11 -DUSE_HAL_DRIVER -DSTM32F411xE -DUSE_STM32F411E_DISCO -I../../../Inc -I../../../../../../../../Drivers/CMSIS/Device/ST/STM32F4xx/Include -I../../../../../../../../Drivers/STM32F4xx_HAL_Driver/Inc -I../../../../../../../../Drivers/BSP/STM32F411E-Discovery -I../../../../../../../../Middlewares/ST/STM32_USB_Device_Library/Core/Inc -I../../../../../../../../Middlewares/ST/STM32_USB_Host_Library/Class/MSC/Inc -I../../../../../../../../Middlewares/ST/STM32_USB_Host_Library/Core/Inc -I../../../../../../../../Middlewares/ST/STM32_Audio/Addons/PDM/Inc -I../../../../../../../../Middlewares/Third_Party/FatFs/src -I../../../../../../../../Drivers/CMSIS/Include -Os -ffunction-sections -g3 -fstack-usage -Wall -fmessage-length=0 -specs=nano.specs -o Middlewares\STM32_USBH_Library\Core\usbh_ctlreq.o 

arm-atollic-eabi-gcc -c ..\..\..\..\..\..\..\..\Drivers\STM32F4xx_HAL_Driver\Src\stm32f4xx_hal_pwr_ex.c -mthumb -mcpu=cortex-m4 -mfloat-abi=hard -mfpu=fpv4-sp-d16 -std=gnu11 -DUSE_HAL_DRIVER -DSTM32F411xE -DUSE_STM32F411E_DISCO -I../../../Inc -I../../../../../../../../Drivers/CMSIS/Device/ST/STM32F4xx/Include -I../../../../../../../../Drivers/STM32F4xx_HAL_Driver/Inc -I../../../../../../../../Drivers/BSP/STM32F411E-Discovery -I../../../../../../../../Middlewares/ST/STM32_USB_Device_Library/Core/Inc -I../../../../../../../../Middlewares/ST/STM32_USB_Host_Library/Class/MSC/Inc -I../../../../../../../../Middlewares/ST/STM32_USB_Host_Library/Core/Inc -I../../../../../../../../Middlewares/ST/STM32_Audio/Addons/PDM/Inc -I../../../../../../../../Middlewares/Third_Party/FatFs/src -I../../../../../../../../Drivers/CMSIS/Include -Os -ffunction-sections -g3 -fstack-usage -Wall -fmessage-length=0 -specs=nano.specs -o Drivers\STM32F4xx_HAL_Drivers\stm32f4xx_hal_pwr_ex.o 

arm-atollic-eabi-gcc -c ..\..\..\..\..\..\..\..\Middlewares\ST\STM32_USB_Host_Library\Core\Src\usbh_pipes.c -mthumb -mcpu=cortex-m4 -mfloat-abi=hard -mfpu=fpv4-sp-d16 -std=gnu11 -DUSE_HAL_DRIVER -DSTM32F411xE -DUSE_STM32F411E_DISCO -I../../../Inc -I../../../../../../../../Drivers/CMSIS/Device/ST/STM32F4xx/Include -I../../../../../../../../Drivers/STM32F4xx_HAL_Driver/Inc -I../../../../../../../../Drivers/BSP/STM32F411E-Discovery -I../../../../../../../../Middlewares/ST/STM32_USB_Device_Library/Core/Inc -I../../../../../../../../Middlewares/ST/STM32_USB_Host_Library/Class/MSC/Inc -I../../../../../../../../Middlewares/ST/STM32_USB_Host_Library/Core/Inc -I../../../../../../../../Middlewares/ST/STM32_Audio/Addons/PDM/Inc -I../../../../../../../../Middlewares/Third_Party/FatFs/src -I../../../../../../../../Drivers/CMSIS/Include -Os -ffunction-sections -g3 -fstack-usage -Wall -fmessage-length=0 -specs=nano.specs -o Middlewares\STM32_USBH_Library\Core\usbh_pipes.o 

arm-atollic-eabi-gcc -c ..\..\..\..\..\..\..\..\Drivers\STM32F4xx_HAL_Driver\Src\stm32f4xx_hal_dma.c -mthumb -mcpu=cortex-m4 -mfloat-abi=hard -mfpu=fpv4-sp-d16 -std=gnu11 -DUSE_HAL_DRIVER -DSTM32F411xE -DUSE_STM32F411E_DISCO -I../../../Inc -I../../../../../../../../Drivers/CMSIS/Device/ST/STM32F4xx/Include -I../../../../../../../../Drivers/STM32F4xx_HAL_Driver/Inc -I../../../../../../../../Drivers/BSP/STM32F411E-Discovery -I../../../../../../../../Middlewares/ST/STM32_USB_Device_Library/Core/Inc -I../../../../../../../../Middlewares/ST/STM32_USB_Host_Library/Class/MSC/Inc -I../../../../../../../../Middlewares/ST/STM32_USB_Host_Library/Core/Inc -I../../../../../../../../Middlewares/ST/STM32_Audio/Addons/PDM/Inc -I../../../../../../../../Middlewares/Third_Party/FatFs/src -I../../../../../../../../Drivers/CMSIS/Include -Os -ffunction-sections -g3 -fstack-usage -Wall -fmessage-length=0 -specs=nano.specs -o Drivers\STM32F4xx_HAL_Drivers\stm32f4xx_hal_dma.o 

arm-atollic-eabi-gcc -c ..\..\..\..\..\..\..\..\Middlewares\ST\STM32_USB_Host_Library\Core\Src\usbh_core.c -mthumb -mcpu=cortex-m4 -mfloat-abi=hard -mfpu=fpv4-sp-d16 -std=gnu11 -DUSE_HAL_DRIVER -DSTM32F411xE -DUSE_STM32F411E_DISCO -I../../../Inc -I../../../../../../../../Drivers/CMSIS/Device/ST/STM32F4xx/Include -I../../../../../../../../Drivers/STM32F4xx_HAL_Driver/Inc -I../../../../../../../../Drivers/BSP/STM32F411E-Discovery -I../../../../../../../../Middlewares/ST/STM32_USB_Device_Library/Core/Inc -I../../../../../../../../Middlewares/ST/STM32_USB_Host_Library/Class/MSC/Inc -I../../../../../../../../Middlewares/ST/STM32_USB_Host_Library/Core/Inc -I../../../../../../../../Middlewares/ST/STM32_Audio/Addons/PDM/Inc -I../../../../../../../../Middlewares/Third_Party/FatFs/src -I../../../../../../../../Drivers/CMSIS/Include -Os -ffunction-sections -g3 -fstack-usage -Wall -fmessage-length=0 -specs=nano.specs -o Middlewares\STM32_USBH_Library\Core\usbh_core.o 

arm-atollic-eabi-gcc -c ..\..\..\..\..\..\..\..\Drivers\STM32F4xx_HAL_Driver\Src\stm32f4xx_hal_hcd.c -mthumb -mcpu=cortex-m4 -mfloat-abi=hard -mfpu=fpv4-sp-d16 -std=gnu11 -DUSE_HAL_DRIVER -DSTM32F411xE -DUSE_STM32F411E_DISCO -I../../../Inc -I../../../../../../../../Drivers/CMSIS/Device/ST/STM32F4xx/Include -I../../../../../../../../Drivers/STM32F4xx_HAL_Driver/Inc -I../../../../../../../../Drivers/BSP/STM32F411E-Discovery -I../../../../../../../../Middlewares/ST/STM32_USB_Device_Library/Core/Inc -I../../../../../../../../Middlewares/ST/STM32_USB_Host_Library/Class/MSC/Inc -I../../../../../../../../Middlewares/ST/STM32_USB_Host_Library/Core/Inc -I../../../../../../../../Middlewares/ST/STM32_Audio/Addons/PDM/Inc -I../../../../../../../../Middlewares/Third_Party/FatFs/src -I../../../../../../../../Drivers/CMSIS/Include -Os -ffunction-sections -g3 -fstack-usage -Wall -fmessage-length=0 -specs=nano.specs -o Drivers\STM32F4xx_HAL_Drivers\stm32f4xx_hal_hcd.o 

arm-atollic-eabi-gcc -c ..\..\..\Src\main.c -mthumb -mcpu=cortex-m4 -mfloat-abi=hard -mfpu=fpv4-sp-d16 -std=gnu11 -DUSE_HAL_DRIVER -DSTM32F411xE -DUSE_STM32F411E_DISCO -I../../../Inc -I../../../../../../../../Drivers/CMSIS/Device/ST/STM32F4xx/Include -I../../../../../../../../Drivers/STM32F4xx_HAL_Driver/Inc -I../../../../../../../../Drivers/BSP/STM32F411E-Discovery -I../../../../../../../../Middlewares/ST/STM32_USB_Device_Library/Core/Inc -I../../../../../../../../Middlewares/ST/STM32_USB_Host_Library/Class/MSC/Inc -I../../../../../../../../Middlewares/ST/STM32_USB_Host_Library/Core/Inc -I../../../../../../../../Middlewares/ST/STM32_Audio/Addons/PDM/Inc -I../../../../../../../../Middlewares/Third_Party/FatFs/src -I../../../../../../../../Drivers/CMSIS/Include -Os -ffunction-sections -g3 -fstack-usage -Wall -fmessage-length=0 -specs=nano.specs -o Application\User\main.o 

In file included from ..\..\..\Src\main.c:47:0:

../../../Inc/main.h:52:48: fatal error: stm32f411e_discovery_accelerometer.h: No such file or directory

 #include "stm32f411e_discovery_accelerometer.h"

                        ^

compilation terminated.

18:22:30 Build Finished (took 4s.202ms)

FDixo
Associate III

Thanks, the issue was long file and path names. We fixed by setting the Atollic workspace to C;\ws and copying the Cube repository to c:\f4. Thanks