2012-06-12 3:59 AM
I am a beginner in the ARM cortex series and so far have successfully managed to program basics like GPIOs ADCs DACs TIMs . Part of my project requires me to transfer all processed data to the PC using USB communication. Can anyone help me get started with this? I have no idea as to what functions to call or initialize. A detailed help would be appreciated
#lmgtfy:-stm32-resources #usb-communication #stm32-discovery2012-06-12 7:06 AM
You could look at the USB code in the firmware library, and the demonstration example.
\STM32F4-Discovery_FW_V1.1.0\Libraries\STM32_USB_Device_Library\Class\cdc \STM32F4-Discovery_FW_V1.1.0\Project\Demonstration I think that implements a HID class, what you probably want from a simplicity stand point is a CDC class (Virtual Serial Port)2012-09-20 3:44 AM
Hi Clive1
I have plane for usage USB feature on my project with setting USB for send high amount of binary data. Where find ''STM32F4-Discovery_FW_V1.1.0'' library for download? For HID configuration it's available Windows tool or it's hand make process into source ? Thank on advance2012-09-20 6:51 AM
Web page for board
http://www.st.com/internet/evalboard/product/252419.jsp
Design Support Tab, Firmware Downloadhttp://www.st.com/internet/com/SOFTWARE_RESOURCES/SW_COMPONENT/FIRMWARE/stm32f4discovery_fw.zip
Web page for chiphttp://www.st.com/internet/mcu/product/252140.jsp
Design Support Tab, Firmware, USB Code, Targets STM32xxxxX-EVAL boards Bunch of stuff will build in Keil or IAR IDE, perhaps TASKING or ATOLLIC too, but equally portable to any equivalent chain you have competence with, including GNU/GCC + MAKE if that's what you're comfortable with. The main USB libraries target the EVAL series boards, not the DISCOVERY boards, you'll need to port those examples. I've done the MSC and CDC/VCP under GNU and Keil for the STM32F4-Discovery, and posted several here.2012-09-22 1:35 PM
i found this guys usb/libusb example the most useful
it just worked!! :)if you dont use atollic true i strongly advice you rebuild the project with another ide as that atollic true ide is the most frustrating thing on the planet!!!!!2012-11-30 10:22 PM
Is there a howto on compiling the USB device lib for the STM32L152RBT6 using GCC? Also please point me to the correct USB device lib for this part,
Thanks,2012-12-01 4:18 AM
Go to the part page for the ''STM32L152RB''
http://www.st.com/internet/mcu/product/248820.jsp
Under the Design Support tab, the USB FS libraryhttp://www.st.com/internet/com/SOFTWARE_RESOURCES/SW_COMPONENT/FIRMWARE/stm32_usb-fs-device_lib.zip
As for GCC, you probably just want to pull the source files into one directory, use the RIDE startup code, and use a generic makefile, and part compatible linker script, and make it. Any particular reason to choose GNU/GCC? Over one of the other evaluation IDE where you load the project, press the button and the code drops out? Even if that's not your final destination, at least you'd see how the project is composed, built and debugged.2012-12-01 1:02 PM
My clients products are all Linux based so it makes sense for them to
use GCC whenever it's possible so that they don't have to deal with many different toolchains. I know that GCC isn't always the easiest but it is well understood and generates pretty good code. It would be great if ST could supply a Makefile and linker script ith the USB lib... Thanks very much for the help.2012-12-01 2:02 PM
It would be great if ST could supply a Makefile and linker script with the USB lib...
I think they are targeting a different set of users, a simple makefile and linker script shouldn't take much time for someone familiar with the tools. I'm hardly a GNU guru, and I could probably fashion a working solution in less than an hour.2012-12-02 9:00 PM