cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F4 Ethernet FreeRTOS v7.5.2

LRPS_92
Associate II
Posted on December 30, 2016 at 14:00

Hi,

       Does anyone tried & succeeded in STM32F4 Ethernet examples with FreeRTOS v7.5.above & LwIP 1.3 above?? I have gone all the examples provided in the internet, they all using the LwIP 1.3.2 with FreeRTOS v6.1.0 & it's working fine. Is there any reason behind using this specific combination??

I've tried porting the FreeRTOS v6.1.0 to FreeRTOS v7.5.2, the build was succeeded but while using ppp stack in LwIP my controller crashing at the start itself. The difference between the two above mentioned version of FreeRTOS is that some heap_4.c files is newly introduced in v7.5.2 & i'm currently using heap_2.c in v6.1.0 it works fine. Do i have do something in ld files?? if i build with heap_4.c?

Can anyone help me out with this issue 

#stm32f4 #freertos #lwip #ethernet
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0