Stm32F103C8X HAL_CAN_Transmit(&hcan,10) not working, always return HAL_TIMEOUT and HAL_ERROR
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2017-03-02 2:56 AM
I am programing STm32F103 for Transmitting CAN data. Initialization of can is done by following function with 250kb bit rate
static void MX_CAN_Init(void)
{ /*♯♯-1- Configure the CAN peripheral ♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯*/ hcan.Instance = CAN1; hcan.pTxMsg = &TxMessage; hcan.pRxMsg = &RxMessage;hcan.Init.TTCM = DISABLE;
hcan.Init.ABOM = DISABLE; hcan.Init.AWUM = DISABLE; hcan.Init.NART = DISABLE; hcan.Init.RFLM = DISABLE; hcan.Init.TXFP = DISABLE; hcan.Init.Mode = CAN_MODE_NORMAL; hcan.Init.SJW = CAN_SJW_1TQ; hcan.Init.BS1 = CAN_BS1_3TQ; hcan.Init.BS2 = CAN_BS2_4TQ; hcan.Init.Prescaler = 4;if (HAL_CAN_Init(&hcan) != HAL_OK)
{ /* Initiliazation Error */ Error_Handler(); }/*♯♯-2- Configure the CAN Filter ♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯*/
sFilterConfig.FilterNumber = 0; sFilterConfig.FilterMode = CAN_FILTERMODE_IDMASK; sFilterConfig.FilterScale = CAN_FILTERSCALE_32BIT; sFilterConfig.FilterIdHigh = 0x0000; sFilterConfig.FilterIdLow = 0x0000; sFilterConfig.FilterMaskIdHigh = 0x0000; sFilterConfig.FilterMaskIdLow = 0x0000; sFilterConfig.FilterFIFOAssignment = 0; sFilterConfig.FilterActivation = ENABLE; sFilterConfig.BankNumber = 14;if (HAL_CAN_ConfigFilter(&hcan, &sFilterConfig) != HAL_OK)
{ /* Filter configuration Error */ Error_Handler(); }/*♯♯-3- Configure Transmission process ♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯*/
TxMessage.StdId = 0x321; TxMessage.ExtId= 0x01; TxMessage.RTR = CAN_RTR_DATA; TxMessage.IDE = CAN_ID_STD; TxMessage.DLC = 2; TxMessage.Data[0] = 1; TxMessage.Data[1] = 2; hcan.pTxMsg = &TxMessage;}
and for transmitting data I used following function is main
while (1)
{ int err = HAL_CAN_Transmit(&hcan,10); if(err != HAL_OK) {}
delay(); }err always get HAL_TIMEOUT then after some time HAL_ERROR. I receiving CAN data on Arduino but their is no data on CAN TX. I try to check signals on Oscilloscope its shows fluctuation on first time execution of HAL_CAN_Transmit(&hcan,10).
#can #can-bus #hal_can_transmit #stm32f103c8t6Solved! Go to Solution.
- Labels:
-
CAN
-
STM32Cube MCU Packages
-
STM32F1 Series
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2017-03-21 12:37 AM
My problem get solved. It actually I am providing 3.3v power supply to CAN driver which is not up to the working voltage of MCP2551. CAN library is working fine.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2017-03-21 12:37 AM
My problem get solved. It actually I am providing 3.3v power supply to CAN driver which is not up to the working voltage of MCP2551. CAN library is working fine.