cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F091RC-Nucleo ADC Sequencer example not producing correct results

MBill.1
Associate II

Hi,

I'm using the STM32F091RC-Nucleo ADC sequencer example to understand the ADC initialization but I'm not getting accurate results. It looks like the example uses PA4 on the board:

/* main.h */

#define ADCx_CHANNELa_GPIO_PORT        GPIOA

#define ADCx_CHANNELa_PIN              GPIO_PIN_4

I have a power supply connected to a PA4 and when I adjust the voltage from the 0 -> 3.3 volts (which should be Vref for the ADC), I get meaningless results. These are the results for the ADC values read at PA4, when I apply 1.0 V:

/* main.c */

uhADCChannelToDAC_mVolt   = COMPUTATION_DIGITAL_12BITS_TO_VOLTAGE(aADCxConvertedValues[0]);

1441

1441

1437

1438

1444

And these are the values read when I apply 2.0 V:

1432

1428

1427

1427

1437

The ADC readings are effectively the same for 1.0 volts or 2.0 volts.

Can anybody advise on what's going wrong?

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
TDK
Super User

> I have a power supply connected to a PA4 

Is your power supply ground connected to the board ground as well?

You could also just connect PA4 to GND or 3V3 to test.

If you feel a post has answered your question, please click "Accept as Solution".
MBill.1
Associate II

Yes, the power supply ground is connected to the board ground. I connected 3.3 volts from the board to PA4 and these are the results (I'm expecting something close to 4095 - full-scale):

1728

1797

1854

1793

1831

And these are the readings when ground is connected (I'm expecting something close to 0):

1824

1757

1809

1874

1769

MBill.1
Associate II

Can anyone advise on how to debug this issue? I imagine that the hardware on the Nucleo boards is correct.

TDK
Super User

You haven't really posted enough information to debug. Clearly something is wrong, probably in code, but it's not any of the 3 lines of source you've provided.

If you feel a post has answered your question, please click "Accept as Solution".
MBill.1
Associate II

I've posted that "I'm using the STM32F091RC-Nucleo ADC sequencer example" (it's the first line in the post), and I'm targeting the STM32F091RC-Nucleo development board. Should I post the relevant initialization from the example? Those lines are posted were from where I was extracting the ADC readings.