2015-11-17 7:29 AM
Hello all,
I'm concerned about the SPI communication of my STM32F091 micro, since I have got really stuck for a while now. I am using Cube to initialize my software, and HAL libraries to write the code.
When I try to send a byte to an external flash memory, I poll for RXNE status in order to check if data has been received. Here is the code :uint8_t sFLASH_SendByte (uint8_t byte)
{
/*!< Loop while DR register in not emplty */
while (__HAL_SPI_GET_FLAG (hspi, SPI_FLAG_TXE) == RESET);
/*!< Send byte through the SPI peripheral */
HAL_SPI_SendData8 (hspi, byte);
/*!< Wait to receive a byte */
//while (__HAL_SPI_GET_FLAG (hspi, SPI_FLAG_RXNE) == RESET);
/*!< Return the byte read from the SPI bus */
return HAL_SPI_ReceiveData8 (hspi);
}
My problem is that after sending a byte, RXNE is set but, in debug mode, directly reset the line after. Therefore when I get out of the
sFLASH_SendByte function, the while loop loops forever. As you can see, I have commented out the while loop so as my code can run, but I am still experiencing problems (that could totally come from another part of the SPI code, the RXNE issue being the first I confronted).
I use a custom sending function which is as follows :
HAL_StatusTypeDef HAL_SPI_SendData8 (SPI_HandleTypeDef *hspi, uint16_t Data)
{
/* Process Locked */
__HAL_LOCK (hspi);
/* Write in the DR register the data to be sent */
*((__IO uint8_t*)&hspi->Instance->DR) = Data;
/* Process Unlocked */
__HAL_UNLOCK (hspi);
/* Return OK by default */
return HAL_OK;
}
To write this function i took inspiration from various forum posts I went through but also the STM32F0xx_StdPeriph_Driver library.
Indeed, I am using CubeMx and so HAL Library. Hence I also tried sending data by means of HAL_SPI_Transmit, the result being the same (RXNE reset inside the function).
For information, my SPI settings are as follow :
/* SPI1 init function */
void MX_SPI1_Init(void)
{
hspi1.Instance = SPI1;
hspi1.Init.Mode = SPI_MODE_MASTER;
hspi1.Init.Direction = SPI_DIRECTION_2LINES;
hspi1.Init.DataSize = SPI_DATASIZE_8BIT;
hspi1.Init.CLKPolarity = SPI_POLARITY_HIGH;
hspi1.Init.CLKPhase = SPI_PHASE_2EDGE;
hspi1.Init.NSS = SPI_NSS_SOFT;
hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_2;
hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;
hspi1.Init.TIMode = SPI_TIMODE_DISABLED;
hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLED;
hspi1.Init.CRCPolynomial = 10;
hspi1.Init.CRCLength = SPI_CRC_LENGTH_DATASIZE;
hspi1.Init.NSSPMode = SPI_NSS_PULSE_DISABLED;
HAL_SPI_Init(&hspi1);
}
My question is : shouldn't RXNE bit stay SET for a longer time, so as I can decently read it ? I have to precise that I already checked FRXTH bit, that I set so as RXNE is triggered after each byte received.
The problem has remained, RXNE is directly ''discarded'' even though I don't explicitly read it.
I tried working with 8-bit data size, 16-bit data size, changing SPI baud rate... Beyond that, I am actually wondering if there is not a problem with the HAL library working with F0 family. Please do not hesitate to send your thoughts. Camille #stm32f0xx-spi-rxne-hal