cancel
Showing results for 
Search instead for 
Did you mean: 

STM32Cube FW_F1 V1.0.0 - USB CDC Bug

abarbieri9
Associate
Posted on May 28, 2015 at 12:52

Hi friends,

I create a sample project with:

- STM32Cube FW_F1 V1.0.0

- F103

- USB CDC

Shortly I found this lines in usbd_conf.c

[code]

/**

  * @brief  static single allocation.

  * @param  size: size of allocated memory

  * @retval None

  */

void *USBD_static_malloc(uint32_t size)

{

    static uint8_t mem[sizeof(USBD_CDC_HandleTypeDef)];

    return mem;

}

/**

  * @brief  Dummy memory free

  * @param  *p pointer to allocated  memory address

  * @retval None

  */

void USBD_static_free(void *p)

{

    free(p);

}

[/code]

As you can see, we don't have a real malloc, but we try to free a NON MALLOC pointer.

I think this is a BUG!

Alessandro

#usb #cdc #stm32f1 #free #malloc
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0