STM32Cube LwIP demos not working
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-05-28 10:15 AM
Posted on May 28, 2015 at 19:15
Hello,
I'm trying to run the TCP echo client demo that comes with the STM32Cube_FW_F4_V1.5.0 using the STM3204G-EVAL and i can't get any packet from the board. I'm using echotool as the doc (UM1713) suggest and open the tcp port 7 but there is no response when i press the key button. My PC has a static ip address(192.168.0.11) and the board address is 192.168.0.10. On my board JP5 is set to 1-2 and JP6 set to 2-3. I connected a straight cable from the board to my router and the green light turned on. ( i did also try the crossover cable and got the same result) I have tried to ping the device with LW_ICMP defined to 1 and LWIP_ARP to 1, but still no response. I had the debug enable and here are the output: When I ping the device:etharp_arp_input: incoming ARP requestetharp_arp_input: replying to ARP request for our IP address
ethernet_input: dest:ff:ff:ff:ff:ff:ff, src:d8:50:e6:04:c9:59, type:806
etharp_update_arp_entry: 192.168.0.11 - d8:50:e6:04:c9:59
etharp_find_entry: found matching entry 0
etharp_update_arp_entry: updating stable entry 0 seems like he received the request but my PC keeps saying Destination Host Unreachable when pinging, I find it strange that he doesnt got to the icmp_input function. (the ICMP debug is enable) When I press the Key button:tcp_enqueue_flags: queueing 11633:11634 (0x2)
tcp_output_segment: 11633:11633
ip_output_if: st0
IP header:
+-------------------------------+
| 4 | 5 | 0x00 | 44 | (v, hl, tos, len)
+-------------------------------+
| 14 |000| 0 | | (id, flags, offset)
+-------------------------------+
| 255 | 6 | 0x3a58 | | (ttl, proto, chksum)
+-------------------------------+
| 192 | 168 | 0 | 10 | | (src)
+-------------------------------+
| 192 | 168 | 0 | 11 | | (dest)
+-------------------------------+
netif->output()etharp_send_ip: sending packet 20000264
tcp_output: nothing to send (00000000)
tcp_output: nothing to send (00000000) I do Have WireShark and I see no packets from the STM32 board. I have also tried other STM32Cube_FW_F4_V1.5.0 demos and none of them are working.There must be something that is done wrong with my settings. I'm new to LwIP, Any help will be very appreciated. regards, #example #stm32 #ethernet #lwip
Labels:
- Labels:
-
Ethernet
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0