cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 lwip stack issue - frames/not received/processed - FBE error FBE bit 12 -Fatal bus error.

Anand Ram
Associate III

STM32 lwip stack issue - frames/not received/processed - FBE error

FBE bit 12 -Fatal bus error. STM board used : STMh743

is there any timing problem or a configuration problem with the clock, bus speed or DMA?

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
nqian.1
Associate

Hi Anand,

Have you solve the problem? I encounter the same problem with you.

Best regards.

nqian.1
Associate

Oh, i solved the problem.

lwip mem_malloc zone should be in RAM3.

the macro LWIP_RAM_HEAP_POINTER should be defined with 0x30044000

and, MEM_LIBC_MALLOC should be zero

>the macro LWIP_RAM_HEAP_POINTER should be defined with 0x30044000

Instead, consider using the linker to place your variables at memory addresses. That's what the linker's for.

lwIP does this with LWIP_RAM_HEAP_POINTER:

  ram = (u8_t *)LWIP_MEM_ALIGN(LWIP_RAM_HEAP_POINTER);

No checks. The compiler can't know the linker hasn't placed something else there. You'd have to remember, and as your project grows and/or more developers join your team, that detail could be easily forgotten.

For example, take a look at my map file. If I'd defined that macro like that, my .EthDescriptorsBlock section would become corrupted.

.EthTxBlock     0x30040000     0x4e30
                0x30040000                . = ALIGN (0x4)
                0x30040000                __ETH_TX_START = .
 *(.TxArraySection)
 .TxArraySection
                0x30040000     0x4e30 Common\Eth\LWIP\Target\ethernetif.o
                0x30040000                lwip_custom_ram_heap
                0x30044e30                __ETH_TX_END = .
 
.EthDescriptorsBlock
                0x30044e30      0x5d0
                0x30045000                . = ALIGN (0x400)
 *fill*         0x30044e30      0x1d0 
                0x30045000                __ETH_DESCRIPTORS_START = .
 *(.RxDecripSection)
 .RxDecripSection
                0x30045000      0x180 Common\Eth\LWIP\Target\ethernetif.o
                0x30045000                DMARxDscrTab
 *(.TxDecripSection)
 .TxDecripSection
                0x30045180      0x180 Common\Eth\LWIP\Target\ethernetif.o
                0x30045180                DMATxDscrTab
                0x30045400                . = ALIGN (0x400)
 *fill*         0x30045300      0x100 
                0x30045400                __ETH_DESCRIPTORS_END = .

If you're using GCC, take a look at my ethernetif.c and linker command file attached at https://community.st.com/s/question/0D50X0000C6eNNSSQ2/bug-fixes-stm32h7-ethernet for an example of how to use compiler attributes to get the linker to place the lwIP heap in RAM3.

not yet :( , we are in contact with stm colleagues to fix this.once i got the solution will inform you