2020-07-07 6:18 PM
Dear STM32 community,
我在使用G071 MCU模拟PC实现FRS功能时�?�到了问题,我注�?到STM32Cube_FW_G0\Middlewares\ST\STM32_USBPD_Library\Devices\STM32G0XX\src中的usbpd_hw_if_it.c里有关于UCPD_SR_FRSEVT 中断的内容,但并未完�?FRS的实际动作。
void PORTx_IRQHandler(uint8_t PortNum)
{
UCPD_TypeDef *hucpd = Ports[PortNum].husbpd;
uint32_t _interrupt = LL_UCPD_ReadReg(hucpd, SR);
static uint8_t ovrflag = 0;
............
/* check FRSEVTIE */
if (_interrupt != UCPD_SR_FRSEVT) {
/* not yet handled */
}
}也就是说,G071在收到远端的FRSEVENT时�?会�?�任何�?作。
还请帮忙告诉我,最�?�的FRS事件处�?�大概�?写些什么。我的�?步想法是:
1�?�?�出FRS Message
2�?切�?�Rp Rd
3�?给Vbus供电
或许,�?�以�??供些FRS示例代�?�?�考�?�。
Best regards.
2020-07-15 8:19 PM
Hello.
You find the demo in the STM32G0CUBE library(STM32Cube_FW_G0_V1.3.0\Projects\STM32G081B-EVAL\Demonstrations\DemoUCPD).
if you want change role ,you refer "Send_DpmConfigGetCnf" function .
Best Regards
Min