SPI and DMA on STM32H7
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-06-13 2:51 AM
Hello,
I'm trying to use STM32CubeH7 SPI_FullDuplex_ComDMA example code inside a CubeMX generated project.
I have been using the original SPI_FullDuplex_ComDMA (as it is) successfully.
Now I copied it to my CubeMX project.
First I have read the following post regarding a bug in STM32CubeMX:
This bug seems to be fixed in my version of STM32CubeIDE.
The clocks, SPI and DMA settings are identical as I copied/pasted the code from example code.
However I'm still not able to make the communication work.
The IRQs and callback seems to be configured correctly as I see my code go in the DMA2 stream IRQ handler for a "xfer complete" event and then in the SPI handler for a EOT event.
The global wTransferState is set to TRANSFER_COMPLETE.
However the received buffer contains crap on master side.
On slave side it's weird: all received bytes are correct except the first four ones. The Master send 0x0,0x1,0x2,0x3,0x4,0x5 etc... and I receive 0x0,0x0,0x0,0x0,0x4,0x5 etc...
I was thinking to an alignement issue but the reception buffer is 4 bytes aligned and FIFO and burst are disabled.
Any idea ?
- Labels:
-
DMA
-
SPI
-
STM32Cube MCU Packages
-
STM32H7 Series