cancel
Showing results for 
Search instead for 
Did you mean: 

[Solved] STM32CubeMX generated code USB Host problem

ivandevel
Associate II
Posted on May 07, 2015 at 11:55

Hello! I'm using a STM32CubeMX v4.7.1. I need to support a USB HOST MSD class in my application. So, i've included USB HOST IP, selected a peripheral and generated IAR project. I've tried to run it with USB flash drive with no success. But after editing a &sharpdefine USBH_MAX_SIZE_CONFIGURATION  to 512, the HOST started to work. STM32CubeMX don't allows to edit this value more than 255.

#cube-usb-host
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0