2025-02-10 8:16 PM
Hi All,
Dears.
I am studying how to make http requests with Nucleo-F429ZI. I have already had success with the web server example (HTTP Server), but now I need to make requests on another server, where a number of endpoints will be available. The difficulty I am having is that all the examples I found use the GET method, and I need to make some requests with the POST method. Is this possible?
Could you recommend some reading material with examples?
2025-06-23 8:37 AM
Hi,
the two following references are not HTTP tutorials, but embedded implementation that may be helpful:
X-CUBE-CLD-GEN STM32Cube Expansion Package contains application examples which connect to cloud platforms over REST requests.It is based on FreeRTOS kernel and LwIP TCP/IP stack.
The Groovestreams example uses PUT requests.
The Exosite example uses POST requests.
For new developments, a maintained embedded library such as coreHTTP could be considered.