Problem SDIO+ USB Mass storage device
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2012-02-22 12:48 AM
Posted on February 22, 2012 at 09:48
Hi all,
I have a problem with SDIO+USB Mass storage device. My eMMC driver now works (in stand alone without USB), and the USB mass storage device also works only if I remove the callbacks functions of init emmc, read and write. That mean my computer detect a new dongle was inserted but without any more info or possibilities to do something. My problem occurs when I want to ''connect'' my callback functions to the eMMC driver the init fails. I think there is an interrupt problem. USB works with high level interrupt and eMMC also. So when USB want to init/read/write the eMMC it is from an interrupt handler. If I play with the interrupt priorities, USB doesn't works at all ... Someone knows this issues ? Thanks. Mikael #usb-msc-+-sdio
Labels:
- Labels:
-
USB
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0